Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum No MAC address on a new Raspberry Pi ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 703 subscribers
  • Views 1583 views
  • Users 0 members are here
  • raspberry
  • address
  • pi
  • ethernet
  • raspberry_pi
  • mac
Related

No MAC address on a new Raspberry Pi ?

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I an new to the Raspberry Pi. I have just received an new Raspberry Pi in a case, with wireless keyboard and Wi-Pi adapter.

 

I am using  a cell phone charger rated at 5V 1A to power the system.

When I boot the Pi with either Ethernet cable or the Wi-Pi adapter I cannot connect to the internet. I've tested the Ethernet cable on another computer and it works.

In the Raspberry Pi settings it shows a MAC address of 00-00-00-00-00-00 (with Ethernet or Wi-Pi adapter). Is this to be expected? I would have expected the adapter (Ethernet or Wi-Pi) to have a MAC address.


Could it be the power supply not supplying enough power to power the network adapter?

 

How do I start a shell window on the Raspberry Pi?


Thanks in advance.

Mark

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks everyone for your helpful suggestions.

     

    I did two things. I bought another charger, this new one rated at 5 volts & 2 Amps and I downloaded and created a Pidora SD card for the Pi.

     

    Initially the Pidora boot wouldn't connect the internet - but in the Ethernet settings for the connection (cabled connection) I cloned the MAC address it found into the settings.

     

    At that point we had a thunderstorm and the nearest broadband cabinent - believe or not - was hit by lightning!! Dead for 24 hours while most of its insides were replaced. Better that than my computers.

     

    After the internet was restored I restarted the Pi-Pidora system, told the router about the MAC address and the Pi was on the net!!!

     

    Conclusion - probably the original power supply wasn't 1 Amp even though  it claimed so, and they system wasn't powering the Ethernet port.

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks everyone for your helpful suggestions.

     

    I did two things. I bought another charger, this new one rated at 5 volts & 2 Amps and I downloaded and created a Pidora SD card for the Pi.

     

    Initially the Pidora boot wouldn't connect the internet - but in the Ethernet settings for the connection (cabled connection) I cloned the MAC address it found into the settings.

     

    At that point we had a thunderstorm and the nearest broadband cabinent - believe or not - was hit by lightning!! Dead for 24 hours while most of its insides were replaced. Better that than my computers.

     

    After the internet was restored I restarted the Pi-Pidora system, told the router about the MAC address and the Pi was on the net!!!

     

    Conclusion - probably the original power supply wasn't 1 Amp even though  it claimed so, and they system wasn't powering the Ethernet port.

     

    Thanks again.