Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO produce sine wave
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 4779 views
  • Users 0 members are here
  • sine
  • pwm
  • raspberry_pi
  • wave
  • pyhton
Related

GPIO produce sine wave

e14 Contributor
e14 Contributor over 12 years ago

Hi

I need the Pi to generate a pulsing sine wave signal. I managed to generate wave signal from the GPIO pin but only square wave with High-Low waveform. So I am wondering if the GPIO can generate the sine wave signal that I need?

Also I have been using the function GPIO.PWM(pin,frequency) i was using it to generate 20kHz signal but when I check the output on oscilloscope it was only 862 Hz is this the maximum frequency of the PWM function or is there something wrong with my pi.

 

I read somewhere the using python Rpi.GPIO library I can output up to around 40 kHz, and I was able to actually output 50 kHz from it but don't know why the it wouldn't output 20 kHz using the GPIO.PWM ().

Can anyone tell me why or suggest another method that I could use?

 

Thank you!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    GPIO.PWM calls the wiringPi library, where the PWM functionality is done in software, i.e. implemented with threads, loops and timers, and therefore this has some limitations. It's really designed to run in the low 100's of Hz, for example setting the brightness of a light or controlling motor speed.  At high frequencies (over 10kHz) the timers are performed with a tight loop, which means the CPU will be at 100% utilization. I don't think you'll get much precision in this situation.

     

    For high frequencies, I think I would be tempted to use a dedicated chip, like the AD9833. This chip has a SPI interface, so should be pretty simple to use with Pi, as it exposes the SDA/SCL pins on the GPIO interface (pins 3,5). This would offload all the hard work from the Pi CPU.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    GPIO.PWM calls the wiringPi library, where the PWM functionality is done in software, i.e. implemented with threads, loops and timers, and therefore this has some limitations. It's really designed to run in the low 100's of Hz, for example setting the brightness of a light or controlling motor speed.  At high frequencies (over 10kHz) the timers are performed with a tight loop, which means the CPU will be at 100% utilization. I don't think you'll get much precision in this situation.

     

    For high frequencies, I think I would be tempted to use a dedicated chip, like the AD9833. This chip has a SPI interface, so should be pretty simple to use with Pi, as it exposes the SDA/SCL pins on the GPIO interface (pins 3,5). This would offload all the hard work from the Pi CPU.