Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO produce sine wave
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 4790 views
  • Users 0 members are here
  • sine
  • pwm
  • raspberry_pi
  • wave
  • pyhton
Related

GPIO produce sine wave

e14 Contributor
e14 Contributor over 12 years ago

Hi

I need the Pi to generate a pulsing sine wave signal. I managed to generate wave signal from the GPIO pin but only square wave with High-Low waveform. So I am wondering if the GPIO can generate the sine wave signal that I need?

Also I have been using the function GPIO.PWM(pin,frequency) i was using it to generate 20kHz signal but when I check the output on oscilloscope it was only 862 Hz is this the maximum frequency of the PWM function or is there something wrong with my pi.

 

I read somewhere the using python Rpi.GPIO library I can output up to around 40 kHz, and I was able to actually output 50 kHz from it but don't know why the it wouldn't output 20 kHz using the GPIO.PWM ().

Can anyone tell me why or suggest another method that I could use?

 

Thank you!

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    what ever method you choose you need to realize that in order to get a decent output waveform with minimal external circuitry you will need to output to a DAC or PWM controller at between 5-10* the frequency you want as output so if your looking to output 20Khz. At a minimum and with assistance with output filters you should follow the Nyquist rate which would specify 2* but that wont give a very clean output.

     

    btw, a simple RC low pass filter will not give a sine wave it will be more like this

    image

    this may be good enough but far from Sine

     

    this is more like what you need

    image

     

    details can be found here http://www.wenzel.com/documents/waveform.html

    but beware this has a resonant frequency and will not work for a wide range of frequencies without varying the values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    what ever method you choose you need to realize that in order to get a decent output waveform with minimal external circuitry you will need to output to a DAC or PWM controller at between 5-10* the frequency you want as output so if your looking to output 20Khz. At a minimum and with assistance with output filters you should follow the Nyquist rate which would specify 2* but that wont give a very clean output.

     

    btw, a simple RC low pass filter will not give a sine wave it will be more like this

    image

    this may be good enough but far from Sine

     

    this is more like what you need

    image

     

    details can be found here http://www.wenzel.com/documents/waveform.html

    but beware this has a resonant frequency and will not work for a wide range of frequencies without varying the values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer