Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Occidentalis Kernel Module for PWM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 707 subscribers
  • Views 3335 views
  • Users 0 members are here
  • raspberry
  • raspberry_pi
  • raspberry-pi
  • kernel
  • raspbian
Related

Occidentalis Kernel Module for PWM

e14 Contributor
e14 Contributor over 12 years ago

Hello!

I'm new to RaspbPi usage and i need to make PWM with a DC Motor.  I have an SD card with NOOBS and have installed Raspbian.

I have a kernel module from the Occidentalis distribution ( from Adafruit) that enables the PI to do that but i don't know how to install it in my PI.

Can anyone help pls?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Iago. I've checked with the lsmod command u said and it shows the pwm module in that list..but i have the following problem when i run the code for controlling a dc motor:

    Error writing to: delayed value: 0

    Error writing to: frequency value: 500

    Error writing to: active value: 1

    Command, f/r/o/p/s 0..9, E.g. f5 :


    this is the code:

    1. import RPi.GPIO as io
    2. io.setmode(io.BCM)
    3. in1_pin = 4
    4. in2_pin = 17
    5. io.setup(in1_pin, io.OUT)
    6. io.setup(in2_pin, io.OUT)
    7. def set(property, value):
    8.    try:
    9.   f = open("/sys/class/rpi-pwm/pwm0/" + property, 'w')
    10.   f.write(value)
    11.   f.close()
    12.    except:
    13.    print("Error writing to: " + property + " value: " + value)
    14. set("delayed", "0")
    15. set("mode", "pwm")
    16. set("frequency", "500")
    17. set("active", "1")
    18. def clockwise():
    19.   io.output(in1_pin, True)  
    20.   io.output(in2_pin, False)
    21. def counter_clockwise():
    22.   io.output(in1_pin, False)
    23.   io.output(in2_pin, True)
    24. clockwise()
    25. while True:
    26.   cmd = raw_input("Command, f/r 0..9, E.g. f5 :")
    27.   direction = cmd[0]
    28.    if direction == "f":
    29.   clockwise()
    30.    else:
    31.   counter_clockwise()
    32.   speed = int(cmd[1]) * 11
    33.    set("duty", str(speed))

    i think here may be the problem : "/sys/class/rpi-pwm/pwm0/" ... it doesn't know that path....i'm runnig Raspbian not Occidentalis...

    Can you help pls?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iagorubio
    0 iagorubio over 12 years ago in reply to e14 Contributor

    can you write here the output of this command ?

     

    sudo ls -al /sys/class/rpi-pwm/pwm0/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • iagorubio
    0 iagorubio over 12 years ago in reply to e14 Contributor

    can you write here the output of this command ?

     

    sudo ls -al /sys/class/rpi-pwm/pwm0/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to iagorubio

    Hey Iago,

    I managed to do the PWM but i've hit another issue...i wanted to control a servomotor and i've pluged it like here:http://learn.adafruit.com/assets/3498 using a 12V power supply...and my Pi just shut down...and now it doesn't boot...my red led stays on and at first the act blinked a little but now nothing...only the red led stays on and i have no output on the monitor...i may have burned it? it was the same power supply used for the dc motor which worked perfectly...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iagorubio
    0 iagorubio over 12 years ago in reply to e14 Contributor

    The servo motor is a completely different beast.

     

    The PWM on the DC motor is used just to limit the voltage on it. So a 50% duty cycle get half the voltage on the motor than a 100% duty cycle.

     

    The PWM on the servo motor, must be a fixed frequency 20ms PWM signal and the high duration on the PWM signal gives the servo the angle it must stay. So if in that 20ms PWM signal the high state is 0.5ms it stays at -90º and if it's 2.5ms it stays at +90º.

     

    Never use a DC motor controller to control servos.

     

    In the other hand 12V seems to be a quite high voltage for a RC servo. They use to go with 6V.

     

    So if the servo was low quality and the 12V voltage "fried" it and it poured into to the the Raspberry's signal wire , there is a high chance of it being dead. The GPIOs on the raspberry are 3.3V tolerant and 12V in there is far too much.

     

    The 12V may be normal for a DC motor as they are more resilient, but the flyback - the EMC voltage when the electric field on the motor coil collapses - can also kill the raspberry, and you may use any kind of IC with built in flyback diodes or some kind of protection.

     

    So what to check:

     

    Is the Servo motor 12V tolerant ?

     

    Is it ok and alive ?

     

    If you don't know if it's 12V tolerant just link it here.

     

    But I am afraid there is a middle to high chance of that Raspberry being dead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to iagorubio

    this is the servo http://www.es.co.th/schemetic/pdf/et-servo-s3003.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    i don't think the servo is dead though...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    or why does the PWR led still stays on and the ACT for reading the SD card sometimes flashes?