Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Small area location tracking?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 676 subscribers
  • Views 795 views
  • Users 0 members are here
  • bluetooth
  • tracking
  • raspberry_pi
  • location
Related

Small area location tracking?

Former Member
Former Member over 11 years ago

Hello Element 14 community,

I was looking for some help in regards to the Raspberry Pi.

I was curious if it is possible to track the location on a mobile phone using bluetooth or something similar.

This would only be in a home, so it wouldn't require long ranges and I would use multiple Pi's.

Also if someone knows if there are any Bluetooth modules available for the Pi that would be really helpful.

Thanks in advance.

  • Sign in to reply
  • Cancel
  • Problemchild
    0 Problemchild over 11 years ago

    All this location determination via Wireless is a rather inexact science. If your location is in the open you may still be able to use GPS(unlikely and probably not accurate enough).

    You could also set up a set of WIFI APs in each room on lower power setting so your phone could use the relative powers of each AP to approximate location. This gives an advantage that you are also providing a method for the data to be sent back to a central source. Bluetooth may be an option but you really need to first ascertain how accurate a position you require.

    I'm afraid the only answer really is to try it out, and at this point  you become the expert in your particular application.

     

    Good luck with your project

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    It should be possible to use Bluetooth 4 (BLE) for short range tracking - the advantage is that the phone doesn't have to pair with the external devices. However, the BLE units seem to be (a) expensive and (b) immature right now.  I had a Red Bear Lab unit that I had to send back already - the radio wasn't on and there didn't seem any useful advice on diagnostics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iagorubio
    0 iagorubio over 11 years ago

    There have been lately some advances in this field with bluetoothLE, but afaik the only working implementation is on iPhone.

     

    Inside iOS 7: iBeacons enhance apps' location awareness via Bluetooth LE

     

    May be you should take a look at it. Looks quite close to what you are looking for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to iagorubio

    ... and that would be iPhone 4s and later, as the earlier ones don't have BLE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    If I wanted to do this project, this is what I would have done.

     

    Create a network of interconnected APs like a mesh.

    When a device gets connected to an AP, it should be able to receive signals from multiple APs at a time.

    Measure the received power at mobile device from each AP.

    If you want to have location of device then have the received power from at least 3 APs.

    I know that is the exact process followed for GPS, but that would be the way I would follow.

    You can find the commands to get the power data from each router in the user manual of router you are using.

     

    You can have a Pi connected to the network and use it to send commands and process the data received.

     

    When you are localizing the device, consider the power attenuated due to walls, doors, etc.

     

    Best of luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Thanks everyone for your help, it is greatly appreciated and will really help with my project