Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Creating an Outdoor Timer That is WiFi or BlueTooth enabled?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 707 subscribers
  • Views 3177 views
  • Users 0 members are here
  • monitoring
  • pi
  • timer
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
Related

Creating an Outdoor Timer That is WiFi or BlueTooth enabled?

vd0gg1t
vd0gg1t over 12 years ago

Hello,


I would like to update my outdoor electric timer switch to be blue toothed/wifi/smartphone enabled.


We have a typical mechanical timer (picture to be taken and attached later today) for our pool pump. This device simply turns the power on or off to the pump depending on the time of day/night. I would like to be able to set this functionality from my mobile device. Additional functionality is desired such as monitoring power draw, indicating clogged pump (heavy draw) or no water (low draw). and even the pi camera to view the basket attached to the pump.


The mobile app I will address elsewhere but the digital interface between the 110 volt circuit and the plug is confusing to me. Could this even be possible with a Pi (or a Pi and other accessories?) It seems possible in theory but in practice that may be another matter.


Thanks,

Vince


  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    Hi Vince,

    Cool idea.

    I just designed a module based on an ARM Cortex M0 that has a Bluetooth interface, a GPS based real time clock and an optically isolated triac output. It also has a light sensor if you want to detect day/night. It could easily be programmed to control the pump schedule and a smart phone could be used to edit the schedule or directly control the pump. If your pump requires more than 1 amp, the the small triac in my module would need to drive a larger external triac or relay. I will likely be blogging about the module here in a week or so, although my application for it is a smart thermostat. I guess you could use a clamp-on current sensor to monitor pump current or you could use pressure sensors to monitor status.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to dougw

    Douglas the Lack of an RTC  would be a pain and I for one have used GPS just for the RTC function however if you

    go for WIFI especially if the device is quite intelligent I would suggest saving the money and using  NTP protocol to set the time maybe even from your local router if  it supports it or more programatically have the GUI control app have the functionality to push the time to the dumb device or have it capable of polling the tablet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 12 years ago in reply to dougw

    Douglas the Lack of an RTC  would be a pain and I for one have used GPS just for the RTC function however if you

    go for WIFI especially if the device is quite intelligent I would suggest saving the money and using  NTP protocol to set the time maybe even from your local router if  it supports it or more programatically have the GUI control app have the functionality to push the time to the dumb device or have it capable of polling the tablet