Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Creating an Outdoor Timer That is WiFi or BlueTooth enabled?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 667 subscribers
  • Views 2396 views
  • Users 0 members are here
  • monitoring
  • pi
  • timer
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
Related

Creating an Outdoor Timer That is WiFi or BlueTooth enabled?

vd0gg1t
vd0gg1t over 11 years ago

Hello,


I would like to update my outdoor electric timer switch to be blue toothed/wifi/smartphone enabled.


We have a typical mechanical timer (picture to be taken and attached later today) for our pool pump. This device simply turns the power on or off to the pump depending on the time of day/night. I would like to be able to set this functionality from my mobile device. Additional functionality is desired such as monitoring power draw, indicating clogged pump (heavy draw) or no water (low draw). and even the pi camera to view the basket attached to the pump.


The mobile app I will address elsewhere but the digital interface between the 110 volt circuit and the plug is confusing to me. Could this even be possible with a Pi (or a Pi and other accessories?) It seems possible in theory but in practice that may be another matter.


Thanks,

Vince


  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    i have been wanting to do this same thing and came up with an idea yesterday and put into use.  i purchased a wifi programmable tstat from honeywell which has an app to be able to control from my phone.i had to install a transformer to power the tstat.    i also used a contactor that is controlled from the tstat y terminal when cool is called for.  the contactor brings on my pump.  so in the program feature of the tstat i call for temp to be 50 deg when i want pump to run and 99 when i want pump to be off .  i also installed a relay that i powered powered with my fan on the tstat or g terminal.  this relay controls my light.  the light is powered on when the relay is unpowered normally closed. on the tstat i leave the fan in on position and so when the pump is off at night i can turn on the light by fan to auto position.  kinda complicated but very simple and excited for the ability for my wife to turn fountains off while in pool with kids during the day by my phone 

     

    wifi tstat

    transformer

    contactor

    relay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    i have been wanting to do this same thing and came up with an idea yesterday and put into use.  i purchased a wifi programmable tstat from honeywell which has an app to be able to control from my phone.i had to install a transformer to power the tstat.    i also used a contactor that is controlled from the tstat y terminal when cool is called for.  the contactor brings on my pump.  so in the program feature of the tstat i call for temp to be 50 deg when i want pump to run and 99 when i want pump to be off .  i also installed a relay that i powered powered with my fan on the tstat or g terminal.  this relay controls my light.  the light is powered on when the relay is unpowered normally closed. on the tstat i leave the fan in on position and so when the pump is off at night i can turn on the light by fan to auto position.  kinda complicated but very simple and excited for the ability for my wife to turn fountains off while in pool with kids during the day by my phone 

     

    wifi tstat

    transformer

    contactor

    relay