Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi + Wolfson + touchscreen LCD ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 681 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Pi + Wolfson + touchscreen LCD ?

e14 Contributor
e14 Contributor over 12 years ago

I've been trying to find the right combination of parts to make a portable audio recorder with digital in.  The wolfson card looks perfect, but I would like to add a touchscreen LCD for start/stop/record/status.  I can't seem to find the right combination of parts, and this would be my first real Pi project.  Can anyone point me in the right direction?  Thanks!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have a similar plan to you (I want to record analogue) but have decided that a screen wouldn't be needed on a portable recorder, and in fact it could be bad - screens use battery life and can break.

     

    Instead I'm planning on doing it using just switches and status LEDs and the only issue I can see is that filenames will have to be randomly generated as recording will always start shortly after power on and with no hardware clock or internet the traditional date formatted names might overwrite...

     

    The switches and LEDs will need to be connected to an I2C expander which should work with the Wolfson but as far as I've read no-one's actually done it.  I have the parts here and will be testing over the weekend - I'll update this thread with my findings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    One of the small TFT touchscreens would be ideal, but the Wolfson card eats up the SPI and all the other GPIO.

    Options:

    HDMI - easiest to use, but bulky interface to larger screens and not so cheap. (HDMIPI)

    DSI - in many ways this is the nicest option, but not available (Due this summer, I think) and not as cheap as small TFTs.

    USB - There are some small 'Sys info' TFT USB displays around, but some are very slow to update (50s for a tiny full-screen image!). If you can work with a small set of icons & text it could be OK.E.g. this.

    There are some USB monitors around, but could support on Pi be a problem?

    SPI - maybe a SPI CS pin can used as a reset by the WAC could be reassigned to an I2C port expander to free one SPI channel. That could enable display on SPI, but not SPI touchscreen. Could be a lot of work.

    I2C - a bit slow for image data, but there are some LCD drivers that will work on I2C for (e.g. RA8875, display + 4-wire resistive touchscreen). Multi-drop bus can wire in parallel with WAC, soldering required.

    Serial - slow, but pins are available on the WAC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Great options!  Thanks for the quick responses.  This is more or less a  "can you do it exercise?" for me.  It's to exercise my brain and learn something new.  Unfortunately, the market has already created almost the perfect device for my needs - M-Audio Microtrack II, which can be had on eBay for less than $50.  Again, thanks for all the responses....I've got some researching to do.