Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi + Wolfson + touchscreen LCD ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 675 subscribers
  • Views 517 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Pi + Wolfson + touchscreen LCD ?

Former Member
Former Member over 11 years ago

I've been trying to find the right combination of parts to make a portable audio recorder with digital in.  The wolfson card looks perfect, but I would like to add a touchscreen LCD for start/stop/record/status.  I can't seem to find the right combination of parts, and this would be my first real Pi project.  Can anyone point me in the right direction?  Thanks!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    One of the small TFT touchscreens would be ideal, but the Wolfson card eats up the SPI and all the other GPIO.

    Options:

    HDMI - easiest to use, but bulky interface to larger screens and not so cheap. (HDMIPI)

    DSI - in many ways this is the nicest option, but not available (Due this summer, I think) and not as cheap as small TFTs.

    USB - There are some small 'Sys info' TFT USB displays around, but some are very slow to update (50s for a tiny full-screen image!). If you can work with a small set of icons & text it could be OK.E.g. this.

    There are some USB monitors around, but could support on Pi be a problem?

    SPI - maybe a SPI CS pin can used as a reset by the WAC could be reassigned to an I2C port expander to free one SPI channel. That could enable display on SPI, but not SPI touchscreen. Could be a lot of work.

    I2C - a bit slow for image data, but there are some LCD drivers that will work on I2C for (e.g. RA8875, display + 4-wire resistive touchscreen). Multi-drop bus can wire in parallel with WAC, soldering required.

    Serial - slow, but pins are available on the WAC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    One of the small TFT touchscreens would be ideal, but the Wolfson card eats up the SPI and all the other GPIO.

    Options:

    HDMI - easiest to use, but bulky interface to larger screens and not so cheap. (HDMIPI)

    DSI - in many ways this is the nicest option, but not available (Due this summer, I think) and not as cheap as small TFTs.

    USB - There are some small 'Sys info' TFT USB displays around, but some are very slow to update (50s for a tiny full-screen image!). If you can work with a small set of icons & text it could be OK.E.g. this.

    There are some USB monitors around, but could support on Pi be a problem?

    SPI - maybe a SPI CS pin can used as a reset by the WAC could be reassigned to an I2C port expander to free one SPI channel. That could enable display on SPI, but not SPI touchscreen. Could be a lot of work.

    I2C - a bit slow for image data, but there are some LCD drivers that will work on I2C for (e.g. RA8875, display + 4-wire resistive touchscreen). Multi-drop bus can wire in parallel with WAC, soldering required.

    Serial - slow, but pins are available on the WAC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer