Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum No display using RCA composite video connector
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 676 subscribers
  • Views 2065 views
  • Users 0 members are here
  • connector
  • raspberry_pi
  • setting
  • display
  • rca
Related

No display using RCA composite video connector

Former Member
Former Member over 11 years ago

Hello,

I have recently purchased a Raspberry Pi and have set it up as follows:

image

 

 

At the TV end I have:

image

I have installed in my first attempt a Kali linux distribution from Download Official Kali Images | Kali Linux Official Documentation which failed and then I downloaded the

NOOBs Lite from Downloads | Raspberry Pi. When I powered on my TV in both cases I have the following result:

image

Similarly for source = AV1, DVD, SVHS, TV I get the same screen.

This is my connector:

image

Kindly help me out.

Thanking you

srikwit

  • Sign in to reply
  • Cancel
Parents
  • crosseyejack
    0 crosseyejack over 11 years ago

    What HDMI to Composite Video cable are you using? It will help better figure out if the cable is compatible

    If you are going to use that cable then you miight need to force HDMI mode. Have a read of Raspberry Pi • View topic - Force HDMI, even if booting w/out HDMI connected You will also need to set a resolution that will match what your TV is expecting though its composite video input, check out RPiconfig - eLinux.org for a list of the video modes you can set the HDMI port to.

     

    And because I have to ask, if you are going to connect the PI using composite video why not just use the composite video out provided by the pi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • crosseyejack
    0 crosseyejack over 11 years ago

    What HDMI to Composite Video cable are you using? It will help better figure out if the cable is compatible

    If you are going to use that cable then you miight need to force HDMI mode. Have a read of Raspberry Pi • View topic - Force HDMI, even if booting w/out HDMI connected You will also need to set a resolution that will match what your TV is expecting though its composite video input, check out RPiconfig - eLinux.org for a list of the video modes you can set the HDMI port to.

     

    And because I have to ask, if you are going to connect the PI using composite video why not just use the composite video out provided by the pi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to crosseyejack

    Hey crosseyjack,

    In my /boot/ I didn't have any config.txt or edid.dat so as per http://www.raspberrypi.org/documentation/configuration/config-txt.md I made a config.txt and a edid.dat as per Raspberry Pi • View topic - Force HDMI, even if booting w/out HDMI connected.

    Contents of config.txt:

    #Normal NTSC

    sdtv_mode=0

    #Video aspect 4:3

    sdtv_aspect =1

    #Maximum HDMI compatibility

    hdmi_safe=1

    #read from edid

    hdmi_edid_file=1

    Contents of edid.dat:

    s plugged in

    /opt/vc/tvservice -d ~/edid.dat

    sudo cp ~/edid.dat /boot

    The result is still the same but some random noise was in AV1 but I think its just noise(I do recognize the post-startx noise of kali).

    Sorry to inform you that it didn't work. Kindly point out my mistakes. Thanks for letting me know about config.txt.