Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum No display using RCA composite video connector
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 675 subscribers
  • Views 2057 views
  • Users 0 members are here
  • connector
  • raspberry_pi
  • setting
  • display
  • rca
Related

No display using RCA composite video connector

Former Member
Former Member over 11 years ago

Hello,

I have recently purchased a Raspberry Pi and have set it up as follows:

image

 

 

At the TV end I have:

image

I have installed in my first attempt a Kali linux distribution from Download Official Kali Images | Kali Linux Official Documentation which failed and then I downloaded the

NOOBs Lite from Downloads | Raspberry Pi. When I powered on my TV in both cases I have the following result:

image

Similarly for source = AV1, DVD, SVHS, TV I get the same screen.

This is my connector:

image

Kindly help me out.

Thanking you

srikwit

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 11 years ago

    Also, unless I'm not seeing it properly, the HDMI to RCA cable as seen in the last photo just looks wrong : ( The HDMI interface only transports digital data, and there doesn't seem to be any electronic adapter box in the photo.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Also, unless I'm not seeing it properly, the HDMI to RCA cable as seen in the last photo just looks wrong : ( The HDMI interface only transports digital data, and there doesn't seem to be any electronic adapter box in the photo.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to shabaz

    Hey shabaz,

    My cable looks similar to http://www.tomshw.it/forum/attachments/schede-audio-altoparlanti-e-cuffie/87805d1385040929-ho-bisogno-di-un-cavo-hdmi-particolare-zena-hdmi-3rca-black-010.jpg

    As you can see, there is no intermediate adapter resulting in a direct conversion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to Former Member

    Perhaps there is some electronics in the black plastic shroud around the HDMI connector. Some active electronics is needed for HDMI to RCA/Composite conversion.

    Anyway, as mentioned by crosseyejack there is no need for this, a two-wire phono/RCA cable is all you need, the RPI has an analog connector on-board that you can use.

    When you get the correct cable, i.e. for analog video, then you will need to press a button while starting up the RPI - see the instructions here.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to shabaz

    Hey shabaz, I connected my raspberry pi to my TV as follows:

    image

    As you can see I have connected the RCA video output of the raspberry pi to the RCA video input of my T.V. and no other connectors are involved. The result is the same. Any suggestion will be helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to Former Member

    Did you press the button on the keyboard as mentioned earlier?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • crosseyejack
    0 crosseyejack over 11 years ago in reply to Former Member

    If you are now using an RCA to RCA cable rename config.txt back to something like config.bak (The config file is optional and is created by NOOBS anyway iirc) and if you like re unpack the NOOBS files on to the SD Card just to make sure you have a "Clean" install to work from.


    As shabaz says BREFORE YOU POWER The Raspberry Pi plug in a USB Keyboard and hold down either the Number 3 or 4 key and power the Raspberry Pi (3 for PAL TV's, 4 for NTSC TV's it all depends on the country you are in. Try 3 first as NTSC TV's will try and display something if given an PAL signal but PAL TV's can not normally handle NTSC signals). Hopefully you should see the NOOBS Setup up screen, at this point you can release the number key you have held down and be able to carry on as normal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer