Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum ISP for AtMega328 on Gertboard
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 708 subscribers
  • Views 1245 views
  • Users 0 members are here
  • usbtinyisp
  • raspberry_pi
  • atmega328
  • gertboard
Related

ISP for AtMega328 on Gertboard

e14 Contributor
e14 Contributor over 12 years ago

I have been looking at using the USBtinyISP from Adafruit for programming the Atmega328 chip on the

Gertboard. As the USBtinyISP has a level-shifter my thought is to power the target chip from the RPI

through J7 by setting a jumper connecting RPIs 3.3V and the 3.3V on the Gertboard.

The result is that all the LEDs on the Gertboard lights up.

Is this a desired behavior?

 

Is there a better way to power it?

 

the USBtinyISP is connected to the board via J23. My goal is to be able to use avr-gcc and avrdude to

program the Atmega328 chip from my laptop directly throught the USBtinyISP.

 

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Please only post one question in one forum if possible, thanks

     

    Now to your question

     

    How are you connecting the ISP programmer to the 328, can you provide a wiring diagram or picture (Or Both) so we can better help you

     

    Thanks

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    image

    This is my setup. I have the jumper on the right in place on J7 to connect the RPis 3.3V to the 3.3V circuit on the Gertboard.

    To get a 'Hello World' example I've connected PB5 to the output and jumper B1 in place to hopefully get LED1 to light up.

     

    But putting in the jumper in J7 all the LEDs lights up.

     

    I had a connection issue posting this question, so I didn't thought the first time went through.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jack.chaney56
    0 jack.chaney56 over 8 years ago in reply to e14 Contributor

    Not sure about the hookups on the Gertboard, but if it is the 6 pin programming port, chances are you are better off providing power to the chip separately. The programmer port does have v+ and gnd listed, however this is more for occasions where the chip is being programmed away from the circuit.  I do a similar operation with an Arduino Nano, and always plug the USB port in to provide power.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jack.chaney56
    0 jack.chaney56 over 8 years ago in reply to e14 Contributor

    Not sure about the hookups on the Gertboard, but if it is the 6 pin programming port, chances are you are better off providing power to the chip separately. The programmer port does have v+ and gnd listed, however this is more for occasions where the chip is being programmed away from the circuit.  I do a similar operation with an Arduino Nano, and always plug the USB port in to provide power.

     

    Jack