Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What are the left GPIOS when using Wolfson Audio Card ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 728 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • audio
  • gpio
  • raspberry_pi
  • raspeberry_pi_accessories
Related

What are the left GPIOS when using Wolfson Audio Card ?

e14 Contributor
e14 Contributor over 12 years ago

I would like to use some gpios for my stuff beside using the wolson audio card, but I can not find which are the GPIO that are still available.

 

Can some one help me about this ?

 

Best Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You can use I2C (I believe the Wolfson card uses I2C as well), however there is no breakout for the I2C pins, so you will have to - at a minimum - solder a few pins to use it. I've successfully driven a RTC and OLED display from the bus, and plan to add a GPIO expander. I went a bit overboard and replaced the header with a stacking header, but I imagine you could solder a few pins to the existing ones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You can use I2C (I believe the Wolfson card uses I2C as well), however there is no breakout for the I2C pins, so you will have to - at a minimum - solder a few pins to use it. I've successfully driven a RTC and OLED display from the bus, and plan to add a GPIO expander. I went a bit overboard and replaced the header with a stacking header, but I imagine you could solder a few pins to the existing ones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Yes, you can do that. See here: Re: Access to 5 GPIO pins with Wolfson Sound Card