Raspberry Pi Forum Connecting the Raspberry Pi to a fixed IP active DHCP server (wi-fi) and 3g network using a dongle simultaneously.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 677 subscribers
  • Views 509 views
  • Users 0 members are here
  • dhcp
  • wifi
  • raspberry_pi
  • raspberrypi
  • 3g
Related

Connecting the Raspberry Pi to a fixed IP active DHCP server (wi-fi) and 3g network using a dongle simultaneously.

Former Member
Former Member over 11 years ago

I'm impressed with the discussions I've seen here over the raspberry Pi.  I'm a software architect and developer I would like to contribute where I can and of course ask for help when I'm at the end of the tunell image

 

 

Ok, i'm new to the Pi and I need to know if it is possible to connect the the Raspberry Pi to a fixed IP active DHCP server (over wi-fi, no internet)  and to a 3g internet network simultaneously.

 

Now both are working independently, that is, it is possible to establish a wi-fi connection using the WiFi edimax adapter and connect to the internet using 3g modem. But, I need to send and receive packets over the (fixed IP to fixed IP) dhcp and at the same time all other applications on the Pi using internet should still work.

 

I would really appreciate any kind of direction image.

 

(The PI is running raspbian OS)

  • Sign in to reply
  • Cancel
  • Problemchild
    0 Problemchild over 11 years ago

    Yes is the answer each interlace is doable and no doubt you'll see examples of each been used individually.

     

    Each will be seen as a separate device and have separate network  configuration  so you can send data to either one or both no problem you will need to configure the routing however if the defaults are not to your liking.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Problemchild

    Assuming that the defaults don't work for you , you'll need to set the routing to send the data for the local subnet to the WIFI( I assume that the WIFI LAN is all on it's own by the sounds) then use the 3G as  default for all other routes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Problemchild

    Thanks a lot John! yes, the WIFI LAN is on its own. I have succesfully connected both interfaces (WiFi and 3g) individually in turn but haven't risked it yet simultaneously.   I will set up my LAN this weekend and give it a try with the defaults.  Ill give an update as soon as i get some results .. and share the steps. thanks again