I'm impressed with the discussions I've seen here over the raspberry Pi. I'm a software architect and developer I would like to contribute where I can and of course ask for help when I'm at the end of the tunell 
Ok, i'm new to the Pi and I need to know if it is possible to connect the the Raspberry Pi to a fixed IP active DHCP server (over wi-fi, no internet) and to a 3g internet network simultaneously.
Now both are working independently, that is, it is possible to establish a wi-fi connection using the WiFi edimax adapter and connect to the internet using 3g modem. But, I need to send and receive packets over the (fixed IP to fixed IP) dhcp and at the same time all other applications on the Pi using internet should still work.
I would really appreciate any kind of direction
.
(The PI is running raspbian OS)