Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Powering via the USB ports
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 6142 views
  • Users 0 members are here
  • b+
  • usb
  • raspberry_pi
  • powering
Related

Powering via the USB ports

e14 Contributor
e14 Contributor over 12 years ago

Have just bought a B+. Reading all the previous documentation on the B indicated I could power the Pi via a USB port if I wanted. I tried this on my B+ and nothing happened !.

 

My particular application has a USB module capable of supplying 2 amps at 5V and will be used for communication with the rest of my system. I do not want to use the micro-usb for power. The connector is inconveniently located and I have no 5V supply apart from the USB module. (This is for an embedded application).

 

Can I use the USB ports for input power on the B+? If not, why not?  The very sparse schematic for the B+ is no help. Is there a more comprehensive one in preparation? It doesn't show the USB ports at all, unlike the one for the B. If there is some 'block' on the USB 5V, could I patch from the USB ports to the 5V pins on the GPIO? (I am a retired professional EE with a long experience of microprocessor systems and quite happy to solder to my Pi if needed). I did note that my mouse, also connected into a USB port, lit up when I connected the power to another USB port - but the Pi itself didn't !

 

Also couldn't find how to send / receive data via a USB port using Python. How does the Pi allocate the USB ports? When booting, my Pi seems to recognise the external USB module  - without installing a driver, which is very surprising as it is a non-standard USB device. How do I check these ports? (Any 'device manager' like Windows?).  I have previously used USB ports as virtual COM ports in Windows. I need to be able to receive and send data (text strings) via a USB from a Python program (or maybe a C# and mono at some stage. Speed may be an issue for me)

 

Regards

 

Mike

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 12 years ago

    Mike,   I happened to plug a Model B into a powered hub and voila the Raspberry Pi started booting. My hub is a 10 port generic USB 2.0 that I got for $11 at an electronics place. Do not know which revision B unless someone tells me how to tell... Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 12 years ago

    Mike,   I happened to plug a Model B into a powered hub and voila the Raspberry Pi started booting. My hub is a 10 port generic USB 2.0 that I got for $11 at an electronics place. Do not know which revision B unless someone tells me how to tell... Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to clem57

    Clem Martins wrote:

     

    Mike,   I happened to plug a Model B into a powered hub and voila the Raspberry Pi started booting. My hub is a 10 port generic USB 2.0 that I got for $11 at an electronics place. Do not know which revision B unless someone tells me how to tell... Clem

    You can see photos of RasPi Model B 1.0 and 2.0 at the RasPi Hardware Wiki: http://elinux.org/RPi_Hardware#Schematic_.2F_Layout

     

    The Model B 1.0 has two polyfuses F1 and F2 next to the USB connector.  They prevent the RasPi from booting reliably with back-powering.  Some users have replaced F1 and F2 with shorts or non-resettable 1A fuses, either of which allows back-powering.  There are a handful of Model B 1.0 PCBs out there manufactured with 0 Ohm jumpers replacing F1 and F2.

     

    The Model B 2.0 does not have polyfuses F1 and F2 and connects USB +5V directly to RasPi's 5V rail.  This allows back-powering, but there's no protection if USB +5V goes bad.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 12 years ago in reply to johnbeetem

    Found revision is B 2.0 made by Sony! by doing cat/proc/cpuinfo Thanks Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to clem57

    Clem

     

    My problem, and original posting, was for the B+. This is significantly different to the B (any version) and doesn't allow back powering as it comes. However, adding the wire as John B suggested does solve the problem.

     

    Mike