Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Powering via the USB ports
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 6130 views
  • Users 0 members are here
  • b+
  • usb
  • raspberry_pi
  • powering
Related

Powering via the USB ports

e14 Contributor
e14 Contributor over 12 years ago

Have just bought a B+. Reading all the previous documentation on the B indicated I could power the Pi via a USB port if I wanted. I tried this on my B+ and nothing happened !.

 

My particular application has a USB module capable of supplying 2 amps at 5V and will be used for communication with the rest of my system. I do not want to use the micro-usb for power. The connector is inconveniently located and I have no 5V supply apart from the USB module. (This is for an embedded application).

 

Can I use the USB ports for input power on the B+? If not, why not?  The very sparse schematic for the B+ is no help. Is there a more comprehensive one in preparation? It doesn't show the USB ports at all, unlike the one for the B. If there is some 'block' on the USB 5V, could I patch from the USB ports to the 5V pins on the GPIO? (I am a retired professional EE with a long experience of microprocessor systems and quite happy to solder to my Pi if needed). I did note that my mouse, also connected into a USB port, lit up when I connected the power to another USB port - but the Pi itself didn't !

 

Also couldn't find how to send / receive data via a USB port using Python. How does the Pi allocate the USB ports? When booting, my Pi seems to recognise the external USB module  - without installing a driver, which is very surprising as it is a non-standard USB device. How do I check these ports? (Any 'device manager' like Windows?).  I have previously used USB ports as virtual COM ports in Windows. I need to be able to receive and send data (text strings) via a USB from a Python program (or maybe a C# and mono at some stage. Speed may be an issue for me)

 

Regards

 

Mike

  • Sign in to reply
  • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to e14 Contributor

    Don't know why it's slower ...In fact what aspect is slow Mike ..Maybe because of it's USB implementation.

    I may say that many other ARM boards running Linux are indeed MUCH faster than the PI and drive GbE with no real problems  so I don't think the move to RiscOS will help much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Problemchild

    John

     

    Having looked closely at the B+, I can't see any Polyfuses except F1 which is the one in the main supply from the power connector. No evidence of any fuses in the supply to / from the USB connectors.However, I can't see where the 5V to the USB connectors comes from. Now if only we had a schematic !

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to e14 Contributor

    I'll need to get mine out and take a more serious look..The poly fuse idea was a punt since the RPI was known for it before

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Problemchild

    John

     

    I was just trying to set up a LAN connection using the Raspbian GUI web browser. Typed in the IP address of my LAN (actually a TP-LINK) and waited ages for an answer. I gave up in the end as it was all so slow.This has nothing to do with the USB as I wasn't using it - except for mouse and keyboard. Doing the same on my laptops, the response is effectively instant.

     

    If other boards running ARM and Linux are so much faster, then we need to ask why? Is this a Pi specific issue? The OS only takes up a bit of the available RAM so access to the SD is not an issue here. (or shouldn't be).

    This is getting off the original topic. Should I start another thread, or is it covered somewhere else? I am new to Pi and its Forums.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to e14 Contributor

    Yep I have the same problem and it seems to be very much a Pi issue as the other Arm boards I use do  not suffer from this.

    The Odroid U3 for example feels like a laptop in use!

     

    I do find the SDcard makes a difference so try that  see if that improves your problem.

     

    Also this is some what off your  original topic so you can create another discussion for this and probably get much more help.

     

    ...you even get more points for doing that image

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    John

     

    Wiring back from the USB connectors to the 'input' end of F1 works a treat. Now powers from the USB side fine. However, the first USB cable I tried gave a voltage drop from the supply (at 5V) of 0.5V at as little as 1 amp and the red light went out. Using another (better) cable there was no measurable drop and the red light was fine. So beware of USB cables.

     

    Anyway, problem solved for me and thanks for your help.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 12 years ago

    Mike,   I happened to plug a Model B into a powered hub and voila the Raspberry Pi started booting. My hub is a 10 port generic USB 2.0 that I got for $11 at an electronics place. Do not know which revision B unless someone tells me how to tell... Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to clem57

    Clem Martins wrote:

     

    Mike,   I happened to plug a Model B into a powered hub and voila the Raspberry Pi started booting. My hub is a 10 port generic USB 2.0 that I got for $11 at an electronics place. Do not know which revision B unless someone tells me how to tell... Clem

    You can see photos of RasPi Model B 1.0 and 2.0 at the RasPi Hardware Wiki: http://elinux.org/RPi_Hardware#Schematic_.2F_Layout

     

    The Model B 1.0 has two polyfuses F1 and F2 next to the USB connector.  They prevent the RasPi from booting reliably with back-powering.  Some users have replaced F1 and F2 with shorts or non-resettable 1A fuses, either of which allows back-powering.  There are a handful of Model B 1.0 PCBs out there manufactured with 0 Ohm jumpers replacing F1 and F2.

     

    The Model B 2.0 does not have polyfuses F1 and F2 and connects USB +5V directly to RasPi's 5V rail.  This allows back-powering, but there's no protection if USB +5V goes bad.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to e14 Contributor

    Mike Bolton wrote:

     

    Wiring back from the USB connectors to the 'input' end of F1 works a treat. Now powers from the USB side fine. However, the first USB cable I tried gave a voltage drop from the supply (at 5V) of 0.5V at as little as 1 amp and the red light went out. Using another (better) cable there was no measurable drop and the red light was fine. So beware of USB cables.

    Peter Oakes wrote an excellent 'blog about RasPi Micro USB power cables and their challenges: http://www.element14.com/community/community/raspberry-pi/blog/2014/03/07/raspberry-pi-usb-power-cables-crashing-and-other-problems

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 12 years ago in reply to johnbeetem

    Found revision is B 2.0 made by Sony! by doing cat/proc/cpuinfo Thanks Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>