Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi B inside a xBox 360 Shell. Power button/lights question?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 1968 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi B inside a xBox 360 Shell. Power button/lights question?

e14 Contributor
e14 Contributor over 11 years ago

Hi

I currently have a raspberry pi B board with a self powered USB hub attached, running two USB hard drives plugged into it. i have it all sitting inside a xbox 360 shell and i was wondering if it is possible to wire up the 4 leds and power button(on the xbox RF module) to the gpio headers on my Pi, so I can push the button and it will turn on my pi and light up the LEDs.

 

I would also like to have everything power off one mains adapter, im guessing i needing to add a power board but which one?

Shutdown circuit (use your own switch) | Mausberry Circuits

https://www.modmypi.com/raspberry-pi-expansion-boards/nwazet-pi-power-supply

 

I hope someone can helpme out.

 

Thanks

 

Mike

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 11 years ago

    You can probably power your RasPi from your hub as long as its external power supply has enough current left over after powering the two hard drives.  All you would need to do is connect a USB cable from one of your hub USB A ports to RasPi's Micro USB power jack.  This assumes that your hub does not have intelligent current control, otherwise it might only supply 100 mA until the device asks for more.  RasPi's power jack only connects +5V and GND, so it can't communicate over the USB data lines.  Usually hubs are dumb about this and just connect all the Vbus signals to a common +5V rail.

     

    I rather like that Mausberry circuit from its description -- I haven't tried it myself.  The circuit is more for turning power off than turning it on -- if you turn off RasPi power without issuing "shutdown" you can corrupt the file system.  The Mausberry circuit and its software should take care of this.

     

    Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    I used to have the pi powered from the hub but I changed back to external power as the pi seemed to struggle. I want the hdd to turn off when I turn the pi off.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    I used to have the pi powered from the hub but I changed back to external power as the pi seemed to struggle. I want the hdd to turn off when I turn the pi off.