Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum MPLAB X and PICkit 3: Failed to get Device ID
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 703 subscribers
  • Views 6164 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

MPLAB X and PICkit 3: Failed to get Device ID

e14 Contributor
e14 Contributor over 11 years ago

Has anyone tried to use MPLAB X IDE v2.30 and PICkit 3 to talk with the chipKIT pi?

 

I created a project and selected this device IC32MX250F128B

 

I then tried to upload (Read Device Memory to File: see http://microchip.wikidot.com/mplabx:read-a-device-and-save-the-hex-file)

 

Here are my results:


*****************************************************

Connecting to MPLAB PICkit 3...
Firmware Suite Version.....01.35.16
Firmware type..............PIC32MX

Target voltage detected
Unable to connect to the target device.
Failed to get Device ID

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I had to set my jumpers different than the defaults:

     

    Default jumper positions:

    JP1 - UART 2 Receive (RX2) (position required to program chipKIT Pi via MPIDE over serial)

    JP4 - UART 2 Transmit (TX2) (position required to program chipKIT Pi via MPIDE over serial)

     

    To use MPLAB X IDE v2.30 and MPLAB IPE with the PICkit 3, set the chipKIT Pi jumpers to these positions

    JP1 - ICSP Function PGEC (C is for clock)

    JP4 - ICSP Function PGED (D is for data)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I had to set my jumpers different than the defaults:

     

    Default jumper positions:

    JP1 - UART 2 Receive (RX2) (position required to program chipKIT Pi via MPIDE over serial)

    JP4 - UART 2 Transmit (TX2) (position required to program chipKIT Pi via MPIDE over serial)

     

    To use MPLAB X IDE v2.30 and MPLAB IPE with the PICkit 3, set the chipKIT Pi jumpers to these positions

    JP1 - ICSP Function PGEC (C is for clock)

    JP4 - ICSP Function PGED (D is for data)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer