Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum MPLAB X and PICkit 3: Failed to get Device ID
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 703 subscribers
  • Views 6163 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

MPLAB X and PICkit 3: Failed to get Device ID

e14 Contributor
e14 Contributor over 11 years ago

Has anyone tried to use MPLAB X IDE v2.30 and PICkit 3 to talk with the chipKIT pi?

 

I created a project and selected this device IC32MX250F128B

 

I then tried to upload (Read Device Memory to File: see http://microchip.wikidot.com/mplabx:read-a-device-and-save-the-hex-file)

 

Here are my results:


*****************************************************

Connecting to MPLAB PICkit 3...
Firmware Suite Version.....01.35.16
Firmware type..............PIC32MX

Target voltage detected
Unable to connect to the target device.
Failed to get Device ID

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    MPLAB IPE fails too with the same error.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    PIC32MX250F128B     http://www.microchip.com.edgekey.net/forums/m731007.aspx

    Pic | Question and Answer - Part 19

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I had to set my jumpers different than the defaults:

     

    Default jumper positions:

    JP1 - UART 2 Receive (RX2) (position required to program chipKIT Pi via MPIDE over serial)

    JP4 - UART 2 Transmit (TX2) (position required to program chipKIT Pi via MPIDE over serial)

     

    To use MPLAB X IDE v2.30 and MPLAB IPE with the PICkit 3, set the chipKIT Pi jumpers to these positions

    JP1 - ICSP Function PGEC (C is for clock)

    JP4 - ICSP Function PGED (D is for data)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Mort
    0 Mort over 3 years ago

    i had been using the microstickii programmer to program pic32mx250f128b  with a pre compiled  hex file for the micromite project. however i fried the micostick ii programmer and had a pickit 3 programmer . at first the pickit3 programmer did not recognize the pic32. somewhere i read that if you hold down the button on the  pickt3 programmer white attaching the programmer to the pc with the mplab ipe ver 5xx the program would load the required operating system to the pickit3

    programmer. hope this helps

    rex