Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Can a Rasbery motherbord control many cameras in a house? How to emplement?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 969 views
  • Users 0 members are here
  • raspberry_pi
  • raspberrypi
  • camera
  • raspeberry_pi_accessories
Related

Can a Rasbery motherbord control many cameras in a house? How to emplement?

e14 Contributor
e14 Contributor over 11 years ago

Can a Rasbery motherbord control many cameras in a house? How to emplement?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Pi can record video from a single USB or IP camera/webcam using free motion capture software like Motion or Xeoma for linux.  Xeoma has added support for linking multiple IPs together so if you have a Pi at every webcam and on your network, you can control all from any Pi or computer.  While Motion is free, Xeoma is technically commercial but it has a free version with some stripped down features.  Still worth checking out.  Both softwares can detect when changes in the picture to trigger recording.  That way you don't fill up your memory card by recording continuously.  If you have a PIR sensor or infrared LED ring for your cameras, you can record in the dark too.  You may be able to get multiple cameras on one Pi (using a powered hub) but usually only at diminished resolutions.  Multiple cameras running anything higher than 640x480 and you'll start to approach the maximum bandwidth for the USB bus regardless of what processor is driving your board.  Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Pi can record video from a single USB or IP camera/webcam using free motion capture software like Motion or Xeoma for linux.  Xeoma has added support for linking multiple IPs together so if you have a Pi at every webcam and on your network, you can control all from any Pi or computer.  While Motion is free, Xeoma is technically commercial but it has a free version with some stripped down features.  Still worth checking out.  Both softwares can detect when changes in the picture to trigger recording.  That way you don't fill up your memory card by recording continuously.  If you have a PIR sensor or infrared LED ring for your cameras, you can record in the dark too.  You may be able to get multiple cameras on one Pi (using a powered hub) but usually only at diminished resolutions.  Multiple cameras running anything higher than 640x480 and you'll start to approach the maximum bandwidth for the USB bus regardless of what processor is driving your board.  Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer