Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Anyone got PiFace Control & Display 2 working with RPi 2 Model B?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 707 subscribers
  • Views 1369 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Anyone got PiFace Control & Display 2 working with RPi 2 Model B?

e14 Contributor
e14 Contributor over 11 years ago

Installed as per instructions here but getting a Python error related to GPIO25 when trying to run sysinfo.py

 

pi@raspberrypi ~ $ sudo python3 /usr/share/doc/python3-pifacecad/examples/sysinfo.py

Traceback (most recent call last):

  File "/usr/lib/python3/dist-packages/pifacecommon/interrupts.py", line 363, in bring_gpio_interrupt_into_userspace

    with open(GPIO_INTERRUPT_DEVICE_VALUE):

IOError: [Errno 2] No such file or directory: '/sys/devices/virtual/gpio/gpio25/value'

 

During handling of the above exception, another exception occurred:

 

Traceback (most recent call last):

  File "/usr/share/doc/python3-pifacecad/examples/sysinfo.py", line 61, in <module>

    cad = pifacecad.PiFaceCAD()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 50, in __init__

    self.init_board()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 87, in init_board

    self.enable_interrupts()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 59, in enable_interrupts

    self.gpio_interrupts_enable()

  File "/usr/lib/python3/dist-packages/pifacecommon/interrupts.py", line 210, in gpio_interrupts_enable

    bring_gpio_interrupt_into_userspace()

  File "/usr/lib/python3/dist-packages/pifacecommon/interrupts.py", line 368, in bring_gpio_interrupt_into_userspace

    export_file.write(str(GPIO_INTERRUPT_PIN))

IOError: [Errno 16] Device or resource busy

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    EDIT: I suspect the problem may be related to the version of Raspian I was using: 2015-01-31-raspbian. I took the SD card out of the RPi 2 Model B and placed it into an older RPi which was known to work with the PiFace CAD 2. A similar error occurred as in the previous post. After downgrading the version of Raspian on the same older model RPi the PiFace CAD 2 then worked. Not sure what to do know whether to wait and see if Raspian gets an update or if the problem lies elsewhere? It would be useful to know if anyone else is having the same problem or if they have PiFace CAD 2 working on RPi 2 Model B running 2015-01-31-raspbian.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Brett,

     

    Thank goodness!

     

    I had a working project. I built a new sd card to increase storage and then the project didn't work showing a very similar error you show above! I thought the piface had failed while I was building the new sd card.

     

    Thanks for posting this. I hope something is sorted soon. Did you say you can downgrade the Raspbian version?

     

    I hope something is sorted soon as I need to finish this project asap and now nothing works!

     

    Chris.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    On my Raspberry Pi B, my internet radio using PiFaceCaD stopped working following the update to the Raspberry Pi 2 kernel.

     

    It appears that with the recent kernel update, the way in which the kernel handles devices has changed with a device tree now being used.

     

    I found this out here - Raspberry Pi • View topic - Breakage after rpi-update? Read this.

     

    I have got my radio working by:

    • sudo raspi-config
    • 8 Advanced Options
    • A5 Device Tree - which I disabled
    • Reboot

     

    My radio now works again image

     

    I assume this will also allow the PiFaceCaD to work with the RPi 2, good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Yes that worked. Thanks so much Simon, really happy the solution was so easy to implement. Much appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Yes that worked for me also. Thank you Simon. Much appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rberk2
    0 rberk2 over 11 years ago

    Hello !

     

    After the latest updates to my rpi 2 mod b

     

    The PIFaceCad and Piface Digital event listeners do not seem to work anymore. Pressing the switches no longer triggers a listener event. My software stopped working, so I tried the example programs, and they do not see switch presses either.

     

    Using the emulators or polling shows the switch states when you press a button on on the real hardware, but any example using listeners does not work any longer on either board ...

     

    The LCD works for write, clear, etc.

     

    Any idea what disabled the interrupts but allows polling of the switches to work. The examples, Like weather, used to work fine.

     

    Both PiFaceCad and PiFaceDigital switch interrupt listeners fail. ( each board is connected to a rpi 2 model b ) Each worked previously.

    Each will show switch states on the emulator, when a button on the real hardware board is pressed.

     

    Thanks !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dongduo
    0 dongduo over 9 years ago in reply to rberk2

    I got the same issue.

    Any solution???