Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Anyone got PiFace Control & Display 2 working with RPi 2 Model B?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 707 subscribers
  • Views 1370 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Anyone got PiFace Control & Display 2 working with RPi 2 Model B?

e14 Contributor
e14 Contributor over 11 years ago

Installed as per instructions here but getting a Python error related to GPIO25 when trying to run sysinfo.py

 

pi@raspberrypi ~ $ sudo python3 /usr/share/doc/python3-pifacecad/examples/sysinfo.py

Traceback (most recent call last):

  File "/usr/lib/python3/dist-packages/pifacecommon/interrupts.py", line 363, in bring_gpio_interrupt_into_userspace

    with open(GPIO_INTERRUPT_DEVICE_VALUE):

IOError: [Errno 2] No such file or directory: '/sys/devices/virtual/gpio/gpio25/value'

 

During handling of the above exception, another exception occurred:

 

Traceback (most recent call last):

  File "/usr/share/doc/python3-pifacecad/examples/sysinfo.py", line 61, in <module>

    cad = pifacecad.PiFaceCAD()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 50, in __init__

    self.init_board()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 87, in init_board

    self.enable_interrupts()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 59, in enable_interrupts

    self.gpio_interrupts_enable()

  File "/usr/lib/python3/dist-packages/pifacecommon/interrupts.py", line 210, in gpio_interrupts_enable

    bring_gpio_interrupt_into_userspace()

  File "/usr/lib/python3/dist-packages/pifacecommon/interrupts.py", line 368, in bring_gpio_interrupt_into_userspace

    export_file.write(str(GPIO_INTERRUPT_PIN))

IOError: [Errno 16] Device or resource busy

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    On my Raspberry Pi B, my internet radio using PiFaceCaD stopped working following the update to the Raspberry Pi 2 kernel.

     

    It appears that with the recent kernel update, the way in which the kernel handles devices has changed with a device tree now being used.

     

    I found this out here - Raspberry Pi • View topic - Breakage after rpi-update? Read this.

     

    I have got my radio working by:

    • sudo raspi-config
    • 8 Advanced Options
    • A5 Device Tree - which I disabled
    • Reboot

     

    My radio now works again image

     

    I assume this will also allow the PiFaceCaD to work with the RPi 2, good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Yes that worked. Thanks so much Simon, really happy the solution was so easy to implement. Much appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Yes that worked. Thanks so much Simon, really happy the solution was so easy to implement. Much appreciated.