Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Piface Digital 2  - InterruptEnableException
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 675 subscribers
  • Views 752 views
  • Users 0 members are here
  • pi
  • raspberry_pi
Related

Piface Digital 2  - InterruptEnableException

Former Member
Former Member over 10 years ago

Hi all

I am VERY new to Raspberry pi and linux in general, so please excuse the noob questions.

 

I have followed the Piface Digital 2 installation instructions to the letter, however receive an interrupt error on line 213 of the Interrupts.py script when I try to run the blink.py script. I am using python 2 by default, but have tried to run the blink.py script under both python 2 and 3. I have attached response in both versions.

At first I thought the problem may relate to the SPI driver, but I have enabled the port and tested it by bridging the MOSI and MISO pins and running spidev_test.c. I receive the correct response.

 

Starting blink.py (or any of the other example programs) with python 2 gives the following result

 

image

 

Starting blink.py with python 3 gives the following result

 

image

 

Any help would be greatly appreciated.

 

Kind regards

Simon

  • Sign in to reply
  • Cancel
  • piface
    0 piface over 10 years ago

    Hi,

     

    This error is due to changes in the new version of Raspbian. The latest package (>v4.1.2)  for python-pifacecommon should fix it. There might be a slight delay as it makes it way through the mirrors, but once that happens, doing a

     

    sudo apt-get update

    sudo apt-get install python{,3}-pifacecommon

    should fix it.

    Regards

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to piface

    Hi Andrew

     

    Thank you very much for the quick response. I have had to return my B+ pi this morning as the spring loaded SD card holder failed. As soon as the replacement arrives I will update pifacecommon and report back.

     

    Kind regards

    Simon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to piface

    Hi Andrew,

    I got exactly the same error as well as soon as i start the pifacedigital-emulator program.. How long will it approx take until the mirrors have been updated? (hours, days, weeks?)

     

    Using:

    • Raspberry Pi 2 (1GB)  & Noobs
    • Piface Digital 2
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • piface
    0 piface over 10 years ago in reply to Former Member

    Should be days at the most. The source is available on github if you want to install from that. https://github.com/piface/pifacecommon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to piface

    Hi Andrew

     

    I finally received the Pi2 and as you predicted the pifacecommon update resolved the problem.

     

    I can now run blink1 and all is fine. I then tried to create a very basic script which set up the input interrupts as per the example and then switch an output on and off based on the status of an input. (When input 1 is pressed then turn on Output 1). This works fine using the GPIO, but not with piface. I have included the script below. I receive an Attribute error: 'int' object has no attribute 'chip'. I am well out of my depth here and no doubt I am making a very obvious error. Your help would be greatly appreciated.

     

     

     

    from time import sleep

    import pifacedigitalio

     

    DELAY = 0.5  # seconds

    pfd = pifacedigitalio.PiFaceDigital() # creates a PiFace Digtal object

     

    def switch_pressed(event):

        event.chip.output_pins[event.pin_num].turn_on()

     

    def switch_unpressed(event):

        event.chip.output_pins[event.pin_num].turn_off()

     

     

    if __name__ == "__main__":

        pifacedigital = pifacedigitalio.PiFaceDigital()

     

        listener = pifacedigitalio.InputEventListener(chip=pifacedigital)

        for i in range(4):

            listener.register(i, pifacedigitalio.IODIR_ON, switch_pressed)

            listener.register(i, pifacedigitalio.IODIR_OFF, switch_unpressed)

        listener.activate()

     

     

        while switch_pressed(1) ==1 :

            pfd.leds[1].turn_on()

        else:

            pfd.leds[1].turn_off()

     

    while True:     #check program is still running by flashing led 3

        pfd.leds[2].toggle()     # toggle third LED

        sleep(DELAY)