Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic Audio Card Enclosure for Pi Model B+ / Pi 2 Model B
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 1617 views
  • Users 0 members are here
  • logic
  • audio
  • cirrus
  • raspberry_pi
  • enclosure
  • raspeberry_pi_accessories
  • card
Related

Cirrus Logic Audio Card Enclosure for Pi Model B+ / Pi 2 Model B

realies
realies over 11 years ago

Hello, I was recently making a research about an enclosure option for the Raspberry Pi Model B+ with the Cirrus Logic audio card but I couldn't really find anything. I was wondering if any of you could have seen something that might work? I own the Pi model B with the Wolfson card and have them equipped with this enclosure (http://uk.farnell.com/camdenboss/wolfson-board-case-carbon/enclosure-box-abs-carbon-fibre/dp/2407263), but apparently the form factor is different and I can't suit it to fit he Model B+ with the Cirrus Logic audio card.

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    I think it is the worth to design one then make it with 3D printer. I am happy to do this (Me too have this audio card) but I have a problem that you other interested users can be helpful to solve. I should know the exact measures for the Pi and the Card, I mean this sort of 3D models of the boards (I have found this for the Arduino for example). With this 3D object it is not so complex to make the perfect enclosure as the internal 3D object is subtracted to the external having all the holes and cuts for the plugs in the right position. Taking manually measures it is a very long operation and not always it is easy to have the exact measure. I have done it for some other boards but the result is always a long time consuming operation needing many experiments with the 3D printer before catching the right internal position.

     

    If someone of you can find these I will prepare the 3D files and post the STL for 3D printing.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marcelheijkoop
    0 marcelheijkoop over 9 years ago in reply to balearicdynamics

    Hi Enrico,

     

    Since the cards are back in use with me , I too am shopping for a case.

    Recently I discovered ready design for laser cut in thingiverse : https://www.thingiverse.com/thing:785289

    And I assume these designs can somehow be used for input in your design.

    In stead of cutting the 6 sides you could pint them as almost 2d objects for x mm thick.

    and now I look again, I also see a 3d print design: https://www.thingiverse.com/thing:1928071

    It is a 3 object set that needs 4 screws and nuts to keep it together.

    With some modifications you could eliminate the use of the original pillars and nylon screws , as the middle object is embraced by the pi and and clac PCB.

    And should be able to supports the boards like the pillars would do

    With the top and bottom lid added to that , correct sized rubber bands could hold it together .

    If you decide to print some, let me know how I can get them too.

    Regards M

    PS: And let's add a few peak holes to see the leds for the  clac and pi 2B and 3B !

    ps2: I see the 3D print design has internal struts for the PCB separation but only at the GPIO side , and would be more useful at the other side.

    Else the outside shell is the only one clamping the 3.5 mm connectors on their barrels.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to marcelheijkoop

    Hello Marcel,

     

    first of all thankyou for the information; I have no longer used my Cirrus Logic audio card but I plan to use it in a project I am working on so with come modifications this case maybe interesting.

     

    Respect to the 3D printed part container all I have found on thingiverse, excluding very few cases is almost usuable. First of all because it is just STL format that is a 3D printing destination and very very difficult to manage with normal CAD applications. Essentially it STL is not. In my opinion the only really efficient use for the 3D STL files is to redesign one (usually with more respect of the 3D printing behaviour and some decent mechanic improvement for robustness) using the STL just as a model reference for holes measures, sizes etc. When the STL is not just theorycal and as a matter of fact it is not printable with good results. In the case you mention is is shown 3D printed so it seems ok as a base for modifications.

    With some modifications you could eliminate the use of the original pillars and nylon screws , as the middle object is embraced by the pi and and clac PCB.

    I should look in depth ow this structure is done and rebuild one but I have liked the project to make it easy to find it later.

     

    About the other project instead based on laser cut acrylic:

    In stead of cutting the 6 sides you could pint them as almost 2d objects for x mm thick.

    Technically it is possible and it has sense. I have done it for a case I had to build very fast when I was in the Netherlands but I was out of acrylic and the small laser cutter was already sent back to home in Spain. Excluding the case when you have not a laser cutter (and material) to be honest I don't see the real advantage to follow this kind of method. But yes, it works and the result is not so bad. Take a look to the images below; I can't open the case to show you all the parts separately as I am using this BBB (old version) in a project.

     

    This is not a very well done enclosure as I have done it with the parts available. You see that the oonger top and bottom layers are not horizontal... It is due the screws that was a bit longer than the needed measure. But it works doing his job image

     

    Enrico

     

    image

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marcelheijkoop
    0 marcelheijkoop over 9 years ago in reply to balearicdynamics

    Hi Enrico,

     

    Unfortunately I have no experience with 3d printers, So I can not transform a description into another, or even know what options there are.

    If you do a first attempt, and it is not 100% what you eventually would have envisioned , it is just a prototype.

    And if it gets the job done, without need to redo the whole process it isn't a bad thing at all.

    Post a picture or thingiverse link if you have created some CLAC enclosure that could benefit more people, like me ;-)

    Regards M.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to marcelheijkoop

    Ok, Anyway I will keep you updated on what I am doing further.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to marcelheijkoop

    Ok, Anyway I will keep you updated on what I am doing further.

     

    Enrico