Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Strange screen artifact
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 712 subscribers
  • Views 3760 views
  • Users 0 members are here
  • raspberrypi
Related

Strange screen artifact

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have 3 Pies

#1  1x Model B with 2 USB ports

#2  1x Model B+ with 4 USB ports

#4  1x Pi2  (there is only one model, right?)

 

I have used all 3 to run Openelec.

#1 works perfectly

#2 and #3 also run openelec but they both show an artifact on the top right-hand corner. It seems to be a miniature version of the colour screen that is shown right after the Pi wakes up but before it runs an OS.

 

Has anyone else seen this????

 

Cheers,

Nick

image

 

image

 

image

  • Sign in to reply
  • Cancel
  • rew
    0 rew over 11 years ago

    Yeah. I've seen this...

     

    I take this logo to mean: "<something> is running" where "<something>" is probably something "videocore", the same thing that does the big square on boot up....

     

    My media center runs on an older 'pi, i.e. your "#1"....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to rew

    Hi Roger,

     

    Which models did you see this on?

    The weird thing is that this is done in both OpenElec and XBian. It almost feels like the firmware did not configure something correctly.

     

    I understand that the initial colourful screen is 4 actual pixels exploded by the GPU to fill the screen.

    The 'logo' I see looks like the GPU has then kept those 4 pixels on but at a smaller magnification factor....weird

     

    Cheers,

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 11 years ago in reply to e14 Contributor

    I'm not "testing pi's if they work as a media center". I'm just "using a pi as a media center". The one I ended up with is the old B (no +). So I have only tested this with one pi, I've seen the square, thought: Hmm. apparently an indication that the GPU is running and forgot about it. It doesn't bother me.

     

    Yes, it looks as if the four pixels are painted and interpolated, for the startup screen blown up to almost fill the screen, while running openelec blown up to say 32x32 pixels or maybe 16x16.

     

    I would think it was put in as a debugging aid to see if the videocore processor is "up and running", it could have been taken out before "shipping" the software, but wasn't. Whether that was intentional or not I don't know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    It's a low-power warning. It shows up when the 5V supply goes below 4.65 if I remember correctly.

    http://www.raspberrypi.org/forums/viewtopic.php?f=29&t=82373

     

    --

    Ragnar

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Good spot! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thank you very much Ragnar!!!!!

    That's exactly what was happening.

     

    I've had issues many years ago with crappy USB leads, so I started buying one at a time from different ebay vendors until I found one that had cables that could carry 2,000 mA and then I bought a dozen or more from him, tested them each and gave most of them to my friends who were complaining about slow charging times.

    (I also bought a bunch for myself)

     

    So, when I saw your message, I collected a few of my 5V, 2,000mA power packs and tested them (as well as 2 different cables) with the Pi2.

    Voila!!!

     

    One substandard cable in the bin later and the Pi is happy.

     

    Thanks again,

    Nick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Glad you got it sorted! image

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 11 years ago in reply to e14 Contributor

    @ Nick

     

    I don't think it is as simple as low capacity power supplies or poor USB leads. In fact, I think the leads either work or don't work. I don't think they have much chance of going high enough resistance at the sorts of current taken by the Pi to stop it working correctly.

     

    Anyway, here's my practical experience. I was getting freezes and a loss of USB with my Pi2 and found that transferring the mouse/keyboard and wifi dongles to a hub powered from the same dual USB PSU as the Pi, solved the problem. I had noticed the rainbow square at times, but not related it to power.

     

    Recently, I decided to try the dongles plugged straight into the Pi and it was fine. The reason was that the (cheapo)  hub supplied power over its USB ports as long as the power was connected and that fed back to the Pi and supplemented the 5V rail. It also lights the red LED even if the Pi is not powered up.

     

    I unplugged the hub from the Pi and rebooted. It worked well, but every time it communicated over the wifi dongle (a very cheap, very short device that probably has to work at full power) the warning rainbow square faded in and out.

     

    The key points are,

     

         1) The hub and the Pi are getting power from the same PSU and so it is not a problem with the power supply lowering the 5V rail under load.

         2) It is unlikely to be a high resistance power lead. I just don't accept that two leads in parallel solve the problem.

     

    The most likely problem is that the internal power arrangements for the Pi are not able to supply the peaks of load from the cheap wifi dongle. It's well known that Wifi is a significant drain of mobile device power, but it will take a bit of pfaffing about with USB PCB sockets and soldered wiring to find out how much this particular dongle is drawing. I may try with an up-market, slightly longer dongle to see if it draws less power, but that needs the IP blacklist on my router to be modified so I am in no rush.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to royleith

    Hi Roy,

    Thanks for the information!

     

    Alas, in my case, I have actually found USB leads in the past that vary a lot, as far as how much current they can carry. (This was done as part of a phone-charging issue....)

    It took me a while to find ones that could carry (very close to ) 2A.

     

    In the case of my Pi, replacing the lead and 5V supply helped fix the rainbow problem. I noticed that just changing the cable made the rainbow appear for a while, fade away, come back and so on....indicating brief outages, as opposed to consistent low-voltage. Once I also changed the PS fixed, it all went away.

     

    I am using a wired-LAN connection, instead of WiFi, so that is not causing me any issues.

     

    If this Pi was used in a critical application, I'd have looked for a nice, regulated 5V supply but, since it is only used as a media center and it works reliably, I'll keep using the little powerpack I have,

    I've got a lot on at the moment, developing software for paying clients, so my hardware itch of getting the multimeter out and measuring resistance in various USB cables, as well as output voltages from the various powerpacks, has been put on hold!

     

    Thanks again,

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to royleith

    OHMS LAW my dear friends OHMS LAW.

     

     

     

    On the newer versions of the Raspbian, there is a core feature that measures the onboard voltage and if it is detected below a set point then the little rainbow square shows up on the top right of the screen, you PI may not crash but it might

     

     

     

    USB Cables come in all sorts of grades and by that I mean how thick the wires are in the cable, under light loads the drop across the cable can be low due to a lower current, as you start spinning up applications or adding load in the form of USB devices plugged directly into the PI, the current increases and therefor the voltage drop increases, I have shown this specifically through experimentation and presented the readings in my post. THE CABLE MATTERS.

     

     

     

    I agree that based on your observations, the power adapter is not lightly to be the issue if everything works when the hub is powered via a separate cable from the power adapter than that of the PI and if you read my blog post on the matter you will see that in all the testing I performed it was never the PSU wall wart.

     

     

     

    Cheap USB hubs that back feed to the PI should not be used especially if the PI is also powered from its own power input, the two can interfere with each other and cause problems, use a better quality HUB.

     

     

     

    Your experience with the WIFI adapter proves my point, as you start to use things  like the WIFI, power consumption goes up (WIFI adapters and most other devices to not consume the same power all the time, it goes up and down depending on how much your asking them to do)

     

     

     

    Powering the PI through a Keyboard USB outlet of from the standard PC USB port may work for low loads but these USB interfaces are nearly always limited to 500mA, not even close to that needed by a busy PI

     

     

     

    Technically two leads in parallel could solve your problem, although impractical the technical result of two resistors in parallel is lower resistance and therefor lower voltage drop for the same current flowing through. In your case it is not really two leads in parallel, one lead is powering the HUB and the connected devices, the other lead it powering the PI, if you have a non-compliant HUB that back feeds to the PI then you will get a partial parallel effect but this is not why it is working better. It is because lower current is flowing in each cable and therefor lower losses before the power gets to the device (PI or HUB)

     

     

     

    You need a Power adapter rated at 1.5A or more for the PI, especially if your adding loads of USB devices, the overall load on the PSU does not change if you separate the load over to cables, you just reduce the risk of dropping too much volts to the PI

     

     

     

    PI 2 will require more power when up and running due to quad core etc. etc. If you still have keyboard, WIFI, and other devices attached, consider a HUB for them and use a 2A Adapter with GOOD quality cables

     

     

     

    I said it at the top and Ill say it again “THE CABLE MATTERS”

     

     

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>