Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi A+ boot problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 693 subscribers
  • Views 1792 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi A+ boot problem

Former Member
Former Member over 11 years ago

I have just received and assembled my Pi A+ and it won't boot. Red power LED on aok, Green ACT LED blinks once then goes out.

Have checked all troubleshooting blogs but no go. Powered up board with SD ejected, and ACT LED comes on, no change when SD inserted. Changed power source and TV. Still no go.

Help!

Using A+ board with Element14 8GB micro SD with NOOBS pre installed, USB attached combo keyboard/mouse, and RCA connector to old Sony TV.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    I have heard of it not getting enough power.  It could also be because of the output settings.  Also try using HDMI as this will work.  Let me know if this helps.

     

    Blakeimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dtsartsanis
    0 dtsartsanis over 11 years ago in reply to Former Member

    Try to power the Pi without a keyboard and mouse. If nothing happens then try another SD card and i would suggested a 8gb.

    Be sure that the power adapter is  5V and 1A and above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dweb98
    0 dweb98 over 11 years ago in reply to dtsartsanis

    Hi, dtsartsanis. First thing. When you are using the Composite (RCA

    Connector) Video Output. You may have to hit either 1 or 2 on your

    Keyboard during Boot-up. It's been a while, since I setup my Pi with

    XBMC Media Player. So, I can't remember which number is for Composite.

    But, each number, is used to Activate a Video Output (Composite or

    HDMI). The default is HDMI. If you don't hit any key, on Boot. After you

    Boot, one time, with Composite Output. Your Pi, may remember your

    selection. Also, I agree with the other Comments. Make sure your OS on

    your SD Card is not Corrupted or the File System is Damaged, too. You

    can do this in any Computer, with a Compatible SD Card Reader. Either

    Built in or External USB Card Reader. I did end up Re-Formatting the

    Pi's SD Card with Noobs and then back again with RaspBMC. I had a little

    problem with the Original File System, that came on the Pre-Formatted

    Element 14 SD Card, becoming Corrupted. And the System Would Not Boot. I

    thought at first that this was because. I had to Hard Shut Down the Pi,

    a couple of times. By Un-Plugging the Power Cord. When I couldn't see

    the OS in the Monitor. During my Tests on using the Analog TV Card to

    input the Signal to a Computer. And when the OS Froze up and would Not

    go to into Shut Down Mode in the GUI. But, Since Reformatting the Card,

    I have not had this Problem again. Through several Hard Shutdowns, since

    then. That was a couple of years ago. I have had to Reformat my SD Card

    twice since then. Initially, I used GParted, a Free and Open Source GUI

    Partition Managing App, that I have been using since about 2005 to

    Repair the File System on the Card. I Put the Card in my Laptop and used

    GParted to Both Repair and Re-Format the SD Card. So, that I would have

    a new and clean file system. Read more in my Article - Review,

    http://www.bishopco.com/2013/10/the-xbmc-raspberry-pi-solution-bundle.html.

    Also, there is more info, on these Pages...

    <http://elinux.org/RPi_Hardware_Basic_Setup#Display>

    RPi Hardware Basic Setup

    http://elinux.org/RPi_Hardware_Basic_Setup#Display

     

    The Raspberry Pi Education Manual (2012 PDF)

    http://pi.cs.man.ac.uk/download/Raspberry_Pi_Education_Manual.pdf

     

    Raspberry Pi - Google Custom Search on DonsDeals Blog

    <http://www.google.com/cse?cx=partner-pub-2221791110207294%3A3qlpn0jxpl8&ie=ISO-8859-1&q=raspberry+pi&sa=Search&siteurl=www.bishopco.com%2F2015%2F03%2Fpi-raq-is-1u-raspberry-pi-based-1u.html&ref=&ss=3839j2395255j13#gsc.tab=0&gsc.q=raspberry%20pi&gsc.page=1>

     

     

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dweb98
    0 dweb98 over 11 years ago in reply to dtsartsanis

    Hi, dtsartsanis. First thing. When you are using the Composite (RCA

    Connector) Video Output. You may have to hit either 1 or 2 on your

    Keyboard during Boot-up. It's been a while, since I setup my Pi with

    XBMC Media Player. So, I can't remember which number is for Composite.

    But, each number, is used to Activate a Video Output (Composite or

    HDMI). The default is HDMI. If you don't hit any key, on Boot. After you

    Boot, one time, with Composite Output. Your Pi, may remember your

    selection. Also, I agree with the other Comments. Make sure your OS on

    your SD Card is not Corrupted or the File System is Damaged, too. You

    can do this in any Computer, with a Compatible SD Card Reader. Either

    Built in or External USB Card Reader. I did end up Re-Formatting the

    Pi's SD Card with Noobs and then back again with RaspBMC. I had a little

    problem with the Original File System, that came on the Pre-Formatted

    Element 14 SD Card, becoming Corrupted. And the System Would Not Boot. I

    thought at first that this was because. I had to Hard Shut Down the Pi,

    a couple of times. By Un-Plugging the Power Cord. When I couldn't see

    the OS in the Monitor. During my Tests on using the Analog TV Card to

    input the Signal to a Computer. And when the OS Froze up and would Not

    go to into Shut Down Mode in the GUI. But, Since Reformatting the Card,

    I have not had this Problem again. Through several Hard Shutdowns, since

    then. That was a couple of years ago. I have had to Reformat my SD Card

    twice since then. Initially, I used GParted, a Free and Open Source GUI

    Partition Managing App, that I have been using since about 2005 to

    Repair the File System on the Card. I Put the Card in my Laptop and used

    GParted to Both Repair and Re-Format the SD Card. So, that I would have

    a new and clean file system. Read more in my Article - Review,

    http://www.bishopco.com/2013/10/the-xbmc-raspberry-pi-solution-bundle.html.

    Also, there is more info, on these Pages...

    <http://elinux.org/RPi_Hardware_Basic_Setup#Display>

    RPi Hardware Basic Setup

    http://elinux.org/RPi_Hardware_Basic_Setup#Display

     

    The Raspberry Pi Education Manual (2012 PDF)

    http://pi.cs.man.ac.uk/download/Raspberry_Pi_Education_Manual.pdf

     

    Raspberry Pi - Google Custom Search on DonsDeals Blog

    <http://www.google.com/cse?cx=partner-pub-2221791110207294%3A3qlpn0jxpl8&ie=ISO-8859-1&q=raspberry+pi&sa=Search&siteurl=www.bishopco.com%2F2015%2F03%2Fpi-raq-is-1u-raspberry-pi-based-1u.html&ref=&ss=3839j2395255j13#gsc.tab=0&gsc.q=raspberry%20pi&gsc.page=1>

     

     

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data