Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Rpi2 cooling
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2904 views
  • Users 0 members are here
  • ram
  • raspi
  • 2
  • temperature
  • overcharge
  • cooler
  • raspberry_pi_2
  • raspberry_pi_space
  • raspberrypi
  • rpi
  • cpu
  • overclocking
  • raspberrypi2
  • cooling
Related

Rpi2 cooling

e14 Contributor
e14 Contributor over 11 years ago

Hello everybody (and sorry for my bad english),

I'm currently working on cooling system for Rpi2 to overclock it a bit. I'm already owner of older model (just B) where are 3 "chips" I'm cooling (CPU/GPU/RAM, ethernet and input voltage regulator) all on front side. On this new B2 model, front side only contains CPU/GPU and ethernet controler and RAM is from bottom side... The question is, if the RAM temperature will increase too, if CPU will be overclocked (i guess yes...)... so is it necessary to cool RAM too? (if there will be a cooler on the bottom of rpi, I would have to mod whole box to fit it in...)

 

Thank you for your help and suggestions.

  • Sign in to reply
  • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to johnbeetem

    "Modern PC boards have BGAs and QFPs, where contact is made by solder balls.  If you stress solder, it doesn't bend -- it cracks.  Eventually the cracks cause intermittent problems, followed by total failure."

     

    Actually QFPs and indeed most "flat" packages do not use solder balls they use leads and even through hole solder connections have been known to crack due to thermal stress and coefficient of

    expansion mismatches. Modern engineers are very aware of these potential problems with BGA and other packages and do their best to prevent it by using the thermal design techniques you speak

    of with impressive results. The only major case of BGA solder ball failure due to thermal stress that I know of was due to a coefficient of expansion problem with a package Nvidia chose for its GPUs,

    clearly without proper thermal design checks. I lost two video cards because of it. There are also other causes for solder balls (and just about every other type of solder joint) failing but these are usually

    manufacturing process problems.

     

     

    "In both cases you need to worry about tin whiskers, thanks to ROHS."

     

    Before ROHS there were tiny solder balls to worry about and before tiny solder balls there were solder bridges. While it has caused quite a few problems, getting rid of lead is a very good thing

    considering the serious disposal and contamination problem it became in our do not repair just replace it and throw the bad one away world.

     

     

    "Or you can run everything cool using good thermal design and avoid these worries."

     

    Yes that is how most boards are designed in the first place and why extra cooling is not needed under normal circumstances..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to gdstew

    Gary Stewart wrote:

     

    While [ROHS] has caused quite a few problems, getting rid of lead is a very good thing considering the serious disposal and contamination problem it became in our do not repair just replace it and throw the bad one away world.

    IMO the "throw away" mentality is a serious problem.  When I was a kid we were sold the idea that when transistors replaced vacuum tubes we would have "solid-state products that lasted forever".  Nowadays you're supposed to throw away your "smart phone" every 2 years and fill landfills with the old ones.  I would rather have reliable lead connections and have electronics that lasts decades and is worth recycling at the end of a long life.  Manufacturers, of course, would like to have you throw away products every two years and they influence governments towards that goal.

     

    JMO/YMMV

     

    P.S. You're right about QFPs.  I had mean to write QFN, the package used by RasPi's USB/LAN chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to gdstew

    Gary Stewart wrote:

     

    The only major case of BGA solder ball failure due to thermal stress that I know of was due to a coefficient of expansion problem with a package Nvidia chose for its GPUs, clearly without proper thermal design checks. I lost two video cards because of it.


    ...


    "Or you can run everything cool using good thermal design and avoid these worries."

     

    Yes that is how most boards are designed in the first place and why extra cooling is not needed under normal circumstances..

    I believe the Xbox 360 had a lot of reliability problems Xbox 360 technical problems - Wikipedia, the free encyclopedia which some have attributed to thermal causes.  According to the Wikipedia link, Microsoft never came clean about the root cause(s).

     

    I've found that a lot of boards, particularly the wonderful cheap little boards we talk about so much here at element14 often have thermal issues.  The original RasPi Model B 1.0 PCB had a design defect which caused some boards' USB/LAN chips to overheat.  This was corrected in the 2.0 PCB, which also has a much better thermal design in general for the USB/LAN.  The Parallella board had a serious overheating problem -- I don't know if they ever really fixed it.  With general-purpose FPGA boards it can be very hard to predict how much power they're going to use.  If you design FPGA logic carefully so that it doesn't do more work than necessary, they can run very cool.  If you design the logic poorly or your application simply requires a lot of signal transitions it can run very hot.

     

    Until very recently Intel has approached chips by making them perform as fast as possible: who cares how much power they use, that's what chip fans are for.  ARM's history was always fan-less, so low power has been a constraint and philosophy from the beginning.  Now that their territories are starting to overlap, Intel is playing catch-up in low power design (Atoms keep getting better) and ARM is learning how to make chips that consume a lot more power to get a little more performance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The issue with overclocking is not temperature. The issue with overclocking is instability due to timing constraints. Overclocking is not recommended. The performance boost you will achieve is minimal, and the possibility for failure due to clocking instability is fantastic.

     

    The whole overclocking thing kinda defeats the purpose behind the Raspberry PI in the first place (a small cool footprint that can be utilized for reliable real world connectivity on the hardware side.

     

    Why are you interested specifically in overclocking?

     

     

    Regards,

    marcus

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<