Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Rpi2 cooling
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2908 views
  • Users 0 members are here
  • ram
  • raspi
  • 2
  • temperature
  • overcharge
  • cooler
  • raspberry_pi_2
  • raspberry_pi_space
  • raspberrypi
  • rpi
  • cpu
  • overclocking
  • raspberrypi2
  • cooling
Related

Rpi2 cooling

e14 Contributor
e14 Contributor over 11 years ago

Hello everybody (and sorry for my bad english),

I'm currently working on cooling system for Rpi2 to overclock it a bit. I'm already owner of older model (just B) where are 3 "chips" I'm cooling (CPU/GPU/RAM, ethernet and input voltage regulator) all on front side. On this new B2 model, front side only contains CPU/GPU and ethernet controler and RAM is from bottom side... The question is, if the RAM temperature will increase too, if CPU will be overclocked (i guess yes...)... so is it necessary to cool RAM too? (if there will be a cooler on the bottom of rpi, I would have to mod whole box to fit it in...)

 

Thank you for your help and suggestions.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Mill a couple blocks of copper or aluminium to sandwich the whole thing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sthibaud
    0 sthibaud over 11 years ago

    Hi,

     

    Sure that overclocking will increase RAM Chip temperature. It is placed on rear face to optimize bus speed with the SoC. Makes cooling more harder.

    But it will depend the overclocking mod that you will apply (frequency and/or voltage, the second will have a bigger impact on temperature)

     

    Without goal of overclocking (as PI2 matches my needs as is), I currently use heatsink on SoC only and Cooling Case with a noiseless tiny fan (powered by GPIO port).

     

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    I have built a few desktop intel computers and can say the memory will heat up, but not to the say degree as the CPU/GPU chips. It will get hotter underneath for sure, so leave some room for air to flow.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago

    For my original 256MB RasPi Model B, I went with an open-frame vertical mount:

    https://community.element14.com/resized-image/__size/310x232/__key/communityserver-discussions-components-files/91/contentimage_5F00_178537.html

    This way I get natural convection cooling on both sides of the board, keeping everything cool with no heat sinks.  You'd have to do the frame differently with a Model B+ or RasPi 2 since they don't have the RCA mounting lug image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    Your minimalist set-up, will have to come up with one for my Rpi 2's. Thanks for the great idea and pics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Your response to my question was excellent. Thank you all for taking the time to reply. I will now mod box and cool ram too. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sthibaud
    0 sthibaud over 11 years ago

    Hi,

     

    It seems also that network chip (usb, ethernet), can heat too.

    Give a look on the thermal pic below. Maybe i will plan to use a second heatsink on it.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to sthibaud

    That is the USB/phys link controller chip.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to clem57

    @ Clem

    It is also the Ethernet controller which uses the USB bus to communicate with the Broadcom SoC.

     

    On the overall subject:

     

    All IC's are designed to run fairly hot. The lowest temperature grade for most ICs is commercial with a maximum die temperature of 70 deg. C (158 deg. F). For

    industrial grade ICs it is 85 deg. C (175 deg. F), and for military grade it is 125 deg. C (250 deg. F, OUCH). Note that even the lowest of these temperatures will

    feel uncomfortably hot on bare skin. I believe that the Broadcom SoCs are industrial grade, if the software is enabled it will throttle the clock when the die reaches

    85 deg. C. If you are overclocking or running it in high ambient temperatures extra cooling is a good idea because it allows the IC package to dissipate the heat of

    the die more efficiently. Otherwise it should be fine as is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to gdstew

    Gary Stewart wrote:

     

    All IC's are designed to run fairly hot. The lowest temperature grade for most ICs is commercial with a maximum die temperature of 70 deg. C (158 deg. F). For industrial grade ICs it is 85 deg. C (175 deg. F), and for military grade it is 125 deg. C (250 deg. F, OUCH). Note that even the lowest of these temperatures will feel uncomfortably hot on bare skin.

    I am a "run it cool" fanatic.

     

    While I realize that the chips can run quite hot safely, high temperature is the enemy of long-term PC board reliability especially if you turn products on and off.  When I got started in this biz, it was mostly through-hole parts or else gull-wing flat packages.  When the board heated up or cooled down, thermal mis-match stresses would be handled by IC package leads.

     

    Modern PC boards have BGAs and QFPs QFNs [*], where contact is made by solder balls [or similar].  If you stress solder, it doesn't bend -- it cracks.  Eventually the cracks cause intermittent problems, followed by total failure.

     

    Of course, you can leave the product turned on all the time, but then your electrolytic capacitors boil away and voltage ripple causes intermittent problems, followed by total failure.

     

    In both cases you need to worry about tin whiskers, thanks to ROHS.

     

    Or you can run everything cool using good thermal design and avoid these worries.

     

    JMO/YMMV

     

    [*] Edit:  I had meant to write QFN (Quad Flat No-leads), not QFP.  As Gary points out below, QFPs are indeed leaded packages and handle thermal stresses nicely.  RasPi uses a QFN for the USB/LAN chip.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>