Raspberry Pi Forum Looking for help on this LCD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 681 subscribers
  • Views 443 views
  • Users 0 members are here
  • lcd
  • raspberry_pi
  • rpi
Related

Looking for help on this LCD

clem57
clem57 over 10 years ago

I am wishing to connect this LCD to a Raspberry Pi using it's LCD interface. I have the data sheet at http://www.beyondinfinite.com/lcd/Library/Hannstar/HSD160PHW1-A.pdf. Can someone point me in the right direction or tell me if this is way off the beat?

Clem

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Clem,

     

    It's not possible directly, because although there is an LCD display connector on the RPI, it is unusable until RPF release some information on it (and when they do, it will be for their displays).

    The display you mention can be used with (say) a HDMI converter circuit board if available.

    Otherwise, better to use it with the RIoTboard, it has a direct interface for connecting up such displays, see these posts, part 1 and part 2.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    Hi Clem,

     

    It's not possible directly, because although there is an LCD display connector on the RPI, it is unusable until RPF release some information on it (and when they do, it will be for their displays).

    The display you mention can be used with (say) a HDMI converter circuit board if available.

    Otherwise, better to use it with the RIoTboard, it has a direct interface for connecting up such displays, see these posts, part 1 and part 2.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer