Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 model B 1 GB hdmi sound problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 4558 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Raspberry Pi 2 model B 1 GB hdmi sound problem

e14 Contributor
e14 Contributor over 11 years ago

Got two of them and same problem on both with several hdmi tv(s). Older Pi worked fine on both tv(s). Headphone jack works fine. Used Python Games to switch as well as sudo raspi-com-fig.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Wait.  Using g the headphone jack?  I believe there was a change to that setup after the first model B.  Something to do with 4 contacts on the jack I stead of 3 (although I think it was more for video and sou d than just sound).  I believe if you pick up one of those special video cables like what most in car systems have, you would be okay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Bill

     

    Have you got into raspi-config and set the option to Force Audio out through HDMI?

    A detailed instruction is available here: https://www.raspberrypi.org/documentation/configuration/audio-config.md

     

    There is also an instruction at the end of the document that you could also try titled "IF YOU'RE STILL NOT GETTING SOUND VIA HDMI"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Bill

     

    Have you got into raspi-config and set the option to Force Audio out through HDMI?

    A detailed instruction is available here: https://www.raspberrypi.org/documentation/configuration/audio-config.md

     

    There is also an instruction at the end of the document that you could also try titled "IF YOU'RE STILL NOT GETTING SOUND VIA HDMI"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    yes did raspi-config from force hdmi to headphones and headphones worked then back to raspi-config to force hdmi and no it did not work

    also tried Python Game sound output and got the same reactions. Also tried some suggestions that involved sudo ... which didn't work.