Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 model B 1 GB hdmi sound problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 4571 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Raspberry Pi 2 model B 1 GB hdmi sound problem

e14 Contributor
e14 Contributor over 11 years ago

Got two of them and same problem on both with several hdmi tv(s). Older Pi worked fine on both tv(s). Headphone jack works fine. Used Python Games to switch as well as sudo raspi-com-fig.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Wait.  Using g the headphone jack?  I believe there was a change to that setup after the first model B.  Something to do with 4 contacts on the jack I stead of 3 (although I think it was more for video and sou d than just sound).  I believe if you pick up one of those special video cables like what most in car systems have, you would be okay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Bill

     

    Have you got into raspi-config and set the option to Force Audio out through HDMI?

    A detailed instruction is available here: https://www.raspberrypi.org/documentation/configuration/audio-config.md

     

    There is also an instruction at the end of the document that you could also try titled "IF YOU'RE STILL NOT GETTING SOUND VIA HDMI"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    yes did raspi-config from force hdmi to headphones and headphones worked then back to raspi-config to force hdmi and no it did not work

    also tried Python Game sound output and got the same reactions. Also tried some suggestions that involved sudo ... which didn't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    my headphones works fine

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    Bill,

         Take a look at http://www.element14.com/community/community/raspberry-pi/raspberrypi2/blog/2015/03/19/see-my-new-pi-2-next-what-should-we-do, It explains the situations of the new Pi 2 may have if the wrong software is installed. I would be glad to assist if you have more questions. One think, are you using the HDMI jack for sure? Because I have directions on composite jack.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Thanks

    I thought this op system could be the problem as I had downloaded it from web on card for my first RPi 2 but for second one - I got the Pi 2 model B camera kit with a Rpi updated 8 gb chip and all is working well except the HDMI sound as indicated above. I can do a jack amplified speaker set with the HDMI screen so that is a solution for now but would love to take new Pi 2 on the road and use other HDMI units (carry least amount of hardware idea) For the old smaller gb Pi - I had no problems with HDMI and I am using the same tv and another (different brand) to try to be sure it's not that. I'm out of town for a few days but will look for others having same problem when back - Thanks you all !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fredt
    0 fredt over 11 years ago

    Hello

     

    I have the same problem.

    Audio does not work

    With larger TV it works but not smaller.

    Jack does not work.

     

    Other parties commented that on load, error is thrown reading tv.

    So it is an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to fredt

    Please start a new question, since your jack does not work.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fredt
    0 fredt over 11 years ago in reply to clem57

    In regards to:

    Please start a new question, since your jack does not work.

     

    Response.

    My HDMI does not work for my smaller HDMI  tv.

    SO I still have an issue.

    The PI is an element14 PI

     

    So I still have a HDMI sound problem

    Plus

    I have a jack problem

     

    These  issues must be tied together.

     

    The resolution other people on the net is to find a HDMI device that works.

    I could not find that again

    but i have this

    ****************

    Go to end or trail for 2015 comments

    https://www.raspberrypi.org/forums/viewtopic.php?f=28&t=62155

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to fredt

    I gave F T 's  larger TV solution a try on the largest tv I have (32" insignia) and got the same ( HDMI no sound ) results I list above with a change from jack ( inland $4.00 headset yes sound ) to forced HDMI using both the sudo raspi-config change and the Python Game sound output change way with no difference. NO HDMI SOUND for me - So what is it with F T 's big set solution for HDMI and my cheep headphone solution for JACK.

     

    Clem Martins

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>