Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Having trouble finding a good power supply for the raspberry pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 2 answers
  • Subscribers 710 subscribers
  • Views 3154 views
  • Users 0 members are here
  • hard_drive
  • raspberry_pi
  • raspberrypi
  • power
Related

Having trouble finding a good power supply for the raspberry pi 2

e14 Contributor
e14 Contributor over 11 years ago

Hi. I just got my raspberry pi 2 a few weeks ago and I'm having trouble finding the best power supply for it. I've tested a few I acquired over the years along with a few other miscellaneous ports.

Below are the various results I've come up with when the USB drive is plugged in. max_usb_current=1 is enabled.

1 - Generic 5V 2A adaptor (Red light blinks on pi, hard drive light stays solid then starts to blink. No sound is heard from drive. Drive is not recognized.)

2 - LG 5.1V 0.7A adaptor (Pi shuts down completely. Drive is not recognized.)

3 - Kyocera 5V 0.8A adaptor (Red light blinks on pi, hard drive lights starts to blink, beeping sound is heard from drive. Drive is not recognized.)

4 - Generic 4.5v-6.5V 0.7A adaptor (No red light on pi, hard drive light stays solid then starts to blink. No sound is heard from drive. Drive is not recognized.)

5 - Plugged into Sanyo TV V/A = ? (No red light on pi, hard drive light blinks momentarily then mounts. Connection to drive is not stable and disconnects after a few minutes or immediately after trying to access it.)

6 - Plugged into computer's USB port V/A = ? (No red light on pi, hard drive light blinks momentarily then mounts. Connection is stable and reliable.)

Yes, I know that last one would work but I thought I'd list it anyway. 4 and 5 seem to be the most interesting to me.

  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    You need to be aware that this power supply outputs 5.3V even though it is rated on the cover of the brick as 5V, Adafruit has deliberatly done this to ensure that at max current with attached cable your still getting 5V at the connector.

     

    5.3V technically EXCEEDS the high limit of 5V logic which is normally rated as 5V +- 5% and that means 4.75V - 5.25V. Generally this should not present any problems but you need to be aware of this as if your only drawing the minimal current then your running the PI at its upper voltage limits.

     

    Most of the logic on the PI actually runs at 3V3 and it has a nice SMPS to get that so it should be tollerent of this higiher voltage. Added devices on the GPIO may not be so forgiving.

     

    Regards

     

    Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • digitaltrousers
    0 digitaltrousers over 11 years ago

    I like the Apple iPad charger, for availability and quality. The first generation was 10W (2A), and the current one is 12W (2.4A). You can get them with free shipping on the Apple Store, although I got my last one on Ebay for about half price. Just make sure it's a genuine one.

    There is some great information at Ken Shirriff's blog:

    http://www.righto.com/2012/10/a-dozen-usb-chargers-in-lab-apple-is.html

    iPad charger teardown: inside Apple's charger and a risky phony

     

    As you're probably aware, when the red light goes out on the Pi, it's an indication that the voltage has dropped below 4.85 (I think) volts. This *can* be due to attempting to draw too much current from the power supply, but as someone else mentioned, it can also be due to the cable (too much resistance), so keep that in mind. Use the best/shortest one you can get.

    I am using the 12W Apple power supply on my Raspberry Pi 2. Originally I had a short micro USB cable connected to a USB extension lead, into the Apple power supply, but I had the issues you mentioned. I changed the cable to a (shorter), single one and now it's fine.

     

    Cheers,

    Dan.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to gdstew

    From what I see, HDD, WiFi, and DVB's seem to need more current than keyboards, mice(wired), and solid state USB sticks.

    gdstew is that not this:

     

    A USB keyboard should use less that 80 mA (0.08A) and a mouse probably about the same. I'm not sure how much current is needed

    for wireless keyboards and mice but it should not be much more.

    TY,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to clem57

    Yes, I was just being a little more specific to show how much difference there is between a hard drive and USB keyboards/mice. Wireless keyboards/mice

    use a lot less power that WiFi because they are used at much shorter ranges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Allright. I got it to work. The supply I bought worked perfectly. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to e14 Contributor

    Excellent ! Now on to bigger and better things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<