Hi,
I have purchase a PiFace from Newark in 2013, it has 26 pins, just wonder, if I buy a new raspberry Pi 2 with 40 pins GPIO, would it compatible with the 26 pin of PiFace card?
Thanks,
-Fu Lee
Hi,
I have purchase a PiFace from Newark in 2013, it has 26 pins, just wonder, if I buy a new raspberry Pi 2 with 40 pins GPIO, would it compatible with the 26 pin of PiFace card?
Thanks,
-Fu Lee
element14Dave please move to Raspberry Pi. Thanks a million.
Clem
Look at https://www.raspberrypi.org/forums/viewtopic.php?f=91&t=104741.
This suggests Piface Digital 2 is needed for Raspberry Pi 2. More information here: Raspberry Pi 2 test, tutorial for upgrade to Raspbian Jessie and WCS working with PiFace
Clem
From a header perspective they both (Piface Digital 1, and Piface Digital 2) should work in the PI2 and the active pins are the same. It uses the SPI bus to talk to a 23S17 16bit port expander and has a ULN2003 open collector driver on seven of the outputs including the two relays.
Physically the PIface Digital 1 will have issues with not fitting over the board nicely and therefor may need tape or other insulation to protect it from shorts and or a header extension. Electrically its compatable. Physically it will fit but precausions are needed
Peter
I seem to recall a similar conversation a few months back
There are some images about the fitment problem, and a solution.
Mark