Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My Pi only outputs DVI, not HDMI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 709 subscribers
  • Views 5307 views
  • Users 0 members are here
  • hdmi
  • raspberry_pi
Related

My Pi only outputs DVI, not HDMI

e14 Contributor
e14 Contributor over 11 years ago

Hi, apologies if this has been answered already but I searched and googled and whilst there were some similar posts around, nothing matched my problem.

I set up my Pi B+ a couple of months ago, initially using a HDMI cable into my TV, then more recently using SSH.  Now I can't get it to output HDMI to the TV anymore.

I've tried various settings in /boot/config.txt but whatever I do the only way I can get it onto a screen is with a passive HDMI to DVI cable.  If I do that then I can select various DVI modes (e.g. 1650x1080 60Hz) but I can't get anything onto a TV by changing the hdmi_group/mode (e.g. 720p) and the TV just says no signal.  I know it's booting up because I can SSH in and if I switch the cable to the HDMI/DVI cable into a monitor then up pops the picture.

I've tried:

hdmi_safe=0 / 1 / unspecified

hdmi_force_hotplug=1

hdmi_drive=1 / 2

config_hdmi_boost=4

2 different TVs

Any help apprecaited

  • Sign in to reply
  • Cancel
Parents
  • amigaamigo
    0 amigaamigo over 11 years ago

    I have had a similar issue with one of my older visio  TVs  changing cables etc didn't work.  I eventually found disconnecting the hdmi cable from the tv unplugging the TV then powering up the TV then the device the problem resolved. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to amigaamigo

    I've tried various combinations of powering down/up - no difference. Thanks anyway image

     

    I have now run a tvservice -n / -M DMT / -m CEA with the pi connected to all three TVs (the one that works plus the two that don't). In all cases I'm getting back identical results ! (see the bottom of this post).

     

    Also been through trying every mode supported (according to the Pioneer manual) - no luck.  Initially I got Group 1 and 2 mixed up (I'm sure they're listed somewhere the other way around !)  So all the modes I tried were group=1 which I hope is CEA.  I did this by modifying config.txt and rebooting.

    Modes tested were :

    Pioneer manual          mode

    1920x1080i@50hz     1, 20

    720*576p@50Hz       1, 17

    1080*720p@50Hz      1, 19

    1920*1080i@60Hz     1, 5

    720*480p@60Hz        1, 2

    1280*720p@60Hz       1, 4


    Nothing worked.


    Here's the output from the tvservice calls (same for all 3 TVs, which sounds unlikely to be correct)

    -----------------------

    device_name=SAM-SyncMaster

    Group DMT has 19 modes:

               mode 4: 640x480 @ 60Hz 4:3, clock:25MHz progressive

               mode 5: 640x480 @ 72Hz 4:3, clock:31MHz progressive

               mode 6: 640x480 @ 75Hz 4:3, clock:31MHz progressive

               mode 8: 800x600 @ 56Hz 4:3, clock:36MHz progressive

               mode 9: 800x600 @ 60Hz 4:3, clock:40MHz progressive

               mode 10: 800x600 @ 72Hz 4:3, clock:50MHz progressive

               mode 11: 800x600 @ 75Hz 4:3, clock:49MHz progressive

               mode 16: 1024x768 @ 60Hz 4:3, clock:65MHz progressive

               mode 17: 1024x768 @ 70Hz 4:3, clock:75MHz progressive

               mode 18: 1024x768 @ 75Hz 4:3, clock:78MHz progressive

               mode 21: 1152x864 @ 75Hz 4:3, clock:108MHz progressive

               mode 28: 1280x800 @ 60Hz 16:10, clock:83MHz progressive

               mode 32: 1280x960 @ 60Hz 4:3, clock:108MHz progressive

               mode 35: 1280x1024 @ 60Hz 5:4, clock:108MHz progressive

               mode 36: 1280x1024 @ 75Hz 5:4, clock:135MHz progressive

               mode 47: 1440x900 @ 60Hz 16:10, clock:106MHz progressive

               mode 48: 1440x900 @ 75Hz 16:10, clock:136MHz progressive

               mode 51: 1600x1200 @ 60Hz 4:3, clock:162MHz progressive

               mode 58: 1680x1050 @ 60Hz 16:10, clock:146MHz progressive

    Group CEA has 14 modes:

               mode 1: 640x480 @ 60Hz 4:3, clock:25MHz progressive

               mode 2: 720x480 @ 60Hz 4:3, clock:27MHz progressive

               mode 3: 720x480 @ 60Hz 16:9, clock:27MHz progressive

               mode 4: 1280x720 @ 60Hz 16:9, clock:74MHz progressive

               mode 5: 1920x1080 @ 60Hz 16:9, clock:74MHz interlaced

      (native) mode 16: 1920x1080 @ 60Hz 16:9, clock:148MHz progressive

               mode 17: 720x576 @ 50Hz 4:3, clock:27MHz progressive

               mode 18: 720x576 @ 50Hz 16:9, clock:27MHz progressive

      (native) mode 19: 1280x720 @ 50Hz 16:9, clock:74MHz progressive

               mode 20: 1920x1080 @ 50Hz 16:9, clock:74MHz interlaced

      (prefer) mode 31: 1920x1080 @ 50Hz 16:9, clock:148MHz progressive

               mode 32: 1920x1080 @ 24Hz 16:9, clock:74MHz progressive

               mode 33: 1920x1080 @ 25Hz 16:9, clock:74MHz progressive

               mode 34: 1920x1080 @ 30Hz 16:9, clock:74MHz progressive

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I know it worked straight out of the box on the Pioneer because I remember sitting in front of it setting it up on Christmas Day 4 months ago.  If anyone can post the default config.txt file (or contents) I'll try that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    disable_overscan=1

    start_x=1

    gpu_mem=128

    From my config.txt

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Thanks for another suggestion. Sadly it didn't help.  If this was my PC I'd assume that some windows update had screwed something up - I assume that apt-get update is not likely to have done something bad ?  If there had been something equivalent to an updated display driver which didn't support HDMI v1.1 any more, and that was pushed put through an update and bundled into all the other OS combinations I've tried it might explain it, but that still wouldn't explain why NOOBS doesn't show either on the TV, would it.  It all sounds rather unlikely.

    Just in case I have gone back to NOOBS (1.3.9) and re-installed Raspbian from that.  No better. I can't find a download of NOOBS 1.3.9 anywhere - it's all 1.4.0 (which I tried and also doesn't work).

    I just can't understand how it worked on 2 TVs and a monitor straight out of the box on Christmas day, but now won't work on any of those, but still works on another TV and monitor, despite reloading everything.  It just sounds like a hardware fault to me.  I'm just about ready to chuck it all back in the box and send it back.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Thanks for another suggestion. Sadly it didn't help.  If this was my PC I'd assume that some windows update had screwed something up - I assume that apt-get update is not likely to have done something bad ?  If there had been something equivalent to an updated display driver which didn't support HDMI v1.1 any more, and that was pushed put through an update and bundled into all the other OS combinations I've tried it might explain it, but that still wouldn't explain why NOOBS doesn't show either on the TV, would it.  It all sounds rather unlikely.

    Just in case I have gone back to NOOBS (1.3.9) and re-installed Raspbian from that.  No better. I can't find a download of NOOBS 1.3.9 anywhere - it's all 1.4.0 (which I tried and also doesn't work).

    I just can't understand how it worked on 2 TVs and a monitor straight out of the box on Christmas day, but now won't work on any of those, but still works on another TV and monitor, despite reloading everything.  It just sounds like a hardware fault to me.  I'm just about ready to chuck it all back in the box and send it back.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Sorry I could not help you. It may be the HDMI 1.1 standard is not supported by newer software on Raspberry Pi. Since you have berry boot, try another OS maybe.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem (and everyone else who had replied),

    Thanks for all the suggestions. I'm going to contact the people I bought it through and see what they have to say.  If I get any solution I'll post it here for info, although I admit the original title is probably not especially helpful given the place I'm at now.

     

    Thanks again

    Tim