Hi,
I'm excited about joining this forum and getting started with Raspberry PI 2. Having a bit of difficulty setting up the SD card. I have already checked to see if the one I have is compatible and it appears to be so. It is a Sony 64gb micro sd card 70mb/s. I have formatted the card using FAT and now I'm about to load the operating system onto the SD card. The instructions call for use of Win32 Disk Imager and downloading the proper OS. I first downloaded Noobs and then I downloaded Noobs Lite. Neither of these contained any .img files needed for writing to the SD card for Win32 Disk Imager. The only .img files in either of the unzipped folders were recovery.img and recovery7.img. Do I use one of these files to write to the SD card or another. Btw, these are the only two file that can be written to the SD card.
Any suggestions?
E