Raspberry Pi Forum Can a SATA to USB converter from an old 5" HD used for SATA SSD ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 684 subscribers
  • Views 565 views
  • Users 0 members are here
  • ssd
  • sata-to-usb
  • usb
  • external-storage
  • raspberry_pi
  • raspberry-pi
  • powering
Related

Can a SATA to USB converter from an old 5" HD used for SATA SSD ?

balearicdynamics
balearicdynamics over 10 years ago

Hi to all.

 

I have got just today the 120 Gb SSD SATA disk that will be the definitive external storage support for the PI master of the Meditech project. At home I have some SATA to USB converter boards recovered from old external USB HDD boxes that hosted 5 inches HD. These boards are powered with 12Vcc and - as I read on the SSD power: +5Vcc I want to be sure that I am not risking to fire immediately the SSD at the first boot.

The two following images shows the front and back of the SSD connected to the board (not yet powered!!!)

 

This is the first time I use an SSD so I really don't know if there are some differences in powering these devices (5Vcc 1,0 A) respect the traditional SATA HDD).

image

image

Thanks in advance. Enrico

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Thanks to all both.

     

    I should admit that this was almost a stupid question. I have used this adaptor with WD 5inches traditional HD but a recent one 1Tb capacity. So I have deducted that it was something like this as the large inductor acting like a real transformer. But I had to be 100% sure so I asked for confirmation.

     

    I have powered the driver just now and it is working correctly. Many thanks for your time.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Thanks to all both.

     

    I should admit that this was almost a stupid question. I have used this adaptor with WD 5inches traditional HD but a recent one 1Tb capacity. So I have deducted that it was something like this as the large inductor acting like a real transformer. But I had to be 100% sure so I asked for confirmation.

     

    I have powered the driver just now and it is working correctly. Many thanks for your time.

     

    Enrico