Raspberry Pi Forum Can a SATA to USB converter from an old 5" HD used for SATA SSD ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 684 subscribers
  • Views 578 views
  • Users 0 members are here
  • ssd
  • sata-to-usb
  • usb
  • external-storage
  • raspberry_pi
  • raspberry-pi
  • powering
Related

Can a SATA to USB converter from an old 5" HD used for SATA SSD ?

balearicdynamics
balearicdynamics over 10 years ago

Hi to all.

 

I have got just today the 120 Gb SSD SATA disk that will be the definitive external storage support for the PI master of the Meditech project. At home I have some SATA to USB converter boards recovered from old external USB HDD boxes that hosted 5 inches HD. These boards are powered with 12Vcc and - as I read on the SSD power: +5Vcc I want to be sure that I am not risking to fire immediately the SSD at the first boot.

The two following images shows the front and back of the SSD connected to the board (not yet powered!!!)

 

This is the first time I use an SSD so I really don't know if there are some differences in powering these devices (5Vcc 1,0 A) respect the traditional SATA HDD).

image

image

Thanks in advance. Enrico

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 10 years ago

    I'm not sure what you want to achieve.

     

    it is likely that the inductor on the PCB (the square black blob near the top on the first picture) is involved in making 5V from the 12V input. That would mean that the USB-5V is not used. Your "laptop format" drive most likely does not use the 12V and only the 5V.

     

    So: This will work, provided you provide a "12V" input on the power jack of the converter.

     

    you're mising "expensive" SSD technology with a "scrapyard" 5.25" usb-sata converter. I don't understand why you'd want to do that. Get a 64G SD card I'd say (can you get 128?). (A scrapyard 3.5" usb-sata converter would be a better fit at least you'd be able to dump the 12V powersupply).

    And again, the SSD is capable of say 200-300Mb/sec of performance, then you're restricting it to about 30Mb/sec by the USB-2 adapter, and then you're conneciting it to the 'pi that has a "not high performing performing" USB subsystem.....

     

    Peter types faster than me... Let me clarify:

    • The SATA drive will only work on 5V


    -> The SATA drive (2.5" formfactor) will work on only 5V.

     

    word-ordering matters. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 10 years ago

    I'm not sure what you want to achieve.

     

    it is likely that the inductor on the PCB (the square black blob near the top on the first picture) is involved in making 5V from the 12V input. That would mean that the USB-5V is not used. Your "laptop format" drive most likely does not use the 12V and only the 5V.

     

    So: This will work, provided you provide a "12V" input on the power jack of the converter.

     

    you're mising "expensive" SSD technology with a "scrapyard" 5.25" usb-sata converter. I don't understand why you'd want to do that. Get a 64G SD card I'd say (can you get 128?). (A scrapyard 3.5" usb-sata converter would be a better fit at least you'd be able to dump the 12V powersupply).

    And again, the SSD is capable of say 200-300Mb/sec of performance, then you're restricting it to about 30Mb/sec by the USB-2 adapter, and then you're conneciting it to the 'pi that has a "not high performing performing" USB subsystem.....

     

    Peter types faster than me... Let me clarify:

    • The SATA drive will only work on 5V


    -> The SATA drive (2.5" formfactor) will work on only 5V.

     

    word-ordering matters. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer