Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPI Pico & ST7789 Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 702 subscribers
  • Views 21289 views
  • Users 0 members are here
  • st7789
  • rpi pico
Related

RPI Pico & ST7789 Display

scottiebabe
scottiebabe over 4 years ago

I purchased an off brand ST7789 1.3" Display a few months ago and recently decided it was time to try it out.

 

I did not realize it at the time but there isn't a consistent pinout between display boards. As it turns out the board I purchased did not pin out the chip-select (CS) line.

 

The ST7789 display driver will function without a CS line, however you need to configure the SPI mode (idle state, edge polarity) to communicate with the display. In most cases, I suppose that would be easy enough to change the display driver.

 

Now I wanted to make use of this display with a PI Pico and Micropython. Pimoroni provide a Micropython release with a small number additional libraries on top of MicroPython : https://github.com/pimoroni/pimoroni-pico (unlike CircuitPython which is significantly different from MicroPython).

 

I was trying to get their example code for one of their displays: https://shop.pimoroni.com/products/1-3-spi-colour-lcd-240x240-breakout to function with my off brand display. Unfortunately, I could not find a way to change the SPI operating mode of the display driver unless I wanted to compile their distribution from source (which I didn't want to do), the SPI initialization was all buried in C code.

 

An intsructables author provided a wonderful guide to breaking out the chip-select line: https://www.instructables.com/Adding-CS-Pin-to-13-LCD/  Many thanks. In the process of modify my display I learned a few things the hard way:

  • Rotated R1 90' to bypass the NPN switch
  • Tossed R2 away and used this as the CS pad
  • Be carful with getting the display too hot. The adhesive that held the display in place virtually no longer exists now image
  • Be carful cleaning! Or don't clean at all. I ended up relocating the flux residue with isopropyl from the PCB to inside the display housing and its now a little merky image

image

 

After the display modifications the display came to life!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have never used one of these displays before, but I have to say I am impressed. I was able to get 35 FPS out of a 240x240 display running over SPI.

 

I still don't know what the best way to add graphics to the PICO is. The image I showed in the video was created with ffmpeg outputting a raw video frame:

 

ffmpeg -vcodec png -i img.png -vcodec rawvideo -f rawvideo -pix_fmt rgb565 img.raw

 

Of this random image cropped down to 240x240:

image

Loading the image from flash was very slow.

 

Update: Image Loading Speed

The framebuffer for the ST7789 is stored big-endian so when I was loading the Image I had endian swap in python which was really slow. I can endian swap the raw image file format using dd:

dd conv=swab if=img.raw of=img2.raw

Now loading the image is now significantly faster:

t1 = time.ticks_us()
with open('img2.raw', 'rb') as f:
    for j in range(0,240,24):
        display_buffer[480*j:(480*(j+24))] = f.read(240*48)

display.update() # only update display once now, remove those tabs!
print((time.ticks_us() - t1)/1000)

 

Which now runs in 232 ms 85 ms and appears more as a transition animation versus terribly slow code.

 

Update: Overclocking in MicroPython

One can adjust the system clock frequency in MicroPython by issuing the following command:

machine.freq(190_000_000) # set system clock in Hz

 

When MicroPython alters the system clock frequency, it also reconfigures the peripheral clock source from clk_sys to the external crystal oscillator.

image

 

So, if you want to maintain a high-speed SPI clock frequency, you need to set the clock mux back to clk_sys yourself by:

mem32[0x40008000+0x48] = 0x800

 

With the Pico running at 190 MHz I achieved the following:

     Rainbow Spinner: 53 FPS

     FFT Demo: 16 FPS

     Image Load + Draw: 56 ms (49ms letting the garbage collector run before the load)

 

Of course, there are no guarantees this will always work for every Pico and or display.

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 4 years ago

    Pimoroni Thermometer Demo

     

    Original source code: https://github.com/pimoroni/pimoroni-pico/blob/main/micropython/examples/pico_display/thermometer.py

     

    I modified this sample application to run on a 240x240 display. This really only involved creating a display object from the 240x240 driver class. I also removed the sleep statement for the demo to run as fast as possible.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Sorry I bumped the board slightly out of focus. This is another neat example of what kind of performance you might see using uPython for graphics on a Pico.

     

    The modified code I used:

    # This example takes the temperature from the Pico's onboard temperature sensor, and displays it on Pico Display Pack, along with a little pixelly graph.
    # It's based on the thermometer example in the "Getting Started with MicroPython on the Raspberry Pi Pico" book, which is a great read if you're a beginner!
    
    from machine import Pin
    import utime
    import gc
    from breakout_colourlcd240x240 import BreakoutColourLCD240x240
    
    rst = Pin(13,Pin.OUT)
    rst.value(1)
    
    width = BreakoutColourLCD240x240.WIDTH
    height = BreakoutColourLCD240x240.HEIGHT
    
    display_buffer = bytearray(width * height * 2)  # 2-bytes per pixel (RGB565)
    display = BreakoutColourLCD240x240(display_buffer)
    
    # reads from Pico's temp sensor and converts it into a more manageable number
    sensor_temp = machine.ADC(4)
    conversion_factor = 3.3 / (65535)
    temp_min = 25
    temp_max = 60
    bar_width = 5
    
    # Set the display backlight to 50%
    display.set_backlight(0.5)
    
    temperatures = []
    
    colors = [(0, 0, 255), (0, 255, 0), (255, 255, 0), (255, 0, 0)]
    
    def temperature_to_color(temp):
        temp = min(temp, temp_max)
        temp = max(temp, temp_min)
    
        f_index = float(temp - temp_min) / float(temp_max - temp_min)
        f_index *= len(colors) - 1
        index = int(f_index)
    
        if index == len(colors) - 1:
            return colors[index]
    
        blend_b = f_index - index
        blend_a = 1.0 - blend_b
    
        a = colors[index]
        b = colors[index + 1]
    
        return [int((a[i] * blend_a) + (b[i] * blend_b)) for i in range(3)]
    
    while True:
        # fills the screen with black
        display.set_pen(0, 0, 0)
        display.clear()
    
        # the following two lines do some maths to convert the number from the temp sensor into celsius
        reading = sensor_temp.read_u16() * conversion_factor
        temperature = 27 - (reading - 0.706) / 0.001721
    
        temperatures.append(temperature)
    
        # shifts the temperatures history to the left by one sample
        if len(temperatures) > width // bar_width:
            temperatures.pop(0)
    
        i = 0
        for t in temperatures:
            # chooses a pen colour based on the temperature
            display.set_pen(*temperature_to_color(t))
    
            # draws the reading as a tall, thin rectangle
            display.rectangle(i, height - ((round(t)-20) * 4), bar_width, height)
    
            # the next tall thin rectangle needs to be drawn
            # "bar_width" (default: 5) pixels to the right of the last one
            i += bar_width
    
        # draws a white background for the text
        display.set_pen(255, 255, 255)
        display.rectangle(1, 1, 100, 25)
    
        # writes the reading as text in the white rectangle
        display.set_pen(0, 0, 0)
        display.text("{:.2f}".format(temperature) + "c", 3, 3, 0, 3)
    
        # time to update the display
        display.update()
    
        # Run Full Speed!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 4 years ago

    Pimoroni Thermometer Demo

     

    Original source code: https://github.com/pimoroni/pimoroni-pico/blob/main/micropython/examples/pico_display/thermometer.py

     

    I modified this sample application to run on a 240x240 display. This really only involved creating a display object from the 240x240 driver class. I also removed the sleep statement for the demo to run as fast as possible.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Sorry I bumped the board slightly out of focus. This is another neat example of what kind of performance you might see using uPython for graphics on a Pico.

     

    The modified code I used:

    # This example takes the temperature from the Pico's onboard temperature sensor, and displays it on Pico Display Pack, along with a little pixelly graph.
    # It's based on the thermometer example in the "Getting Started with MicroPython on the Raspberry Pi Pico" book, which is a great read if you're a beginner!
    
    from machine import Pin
    import utime
    import gc
    from breakout_colourlcd240x240 import BreakoutColourLCD240x240
    
    rst = Pin(13,Pin.OUT)
    rst.value(1)
    
    width = BreakoutColourLCD240x240.WIDTH
    height = BreakoutColourLCD240x240.HEIGHT
    
    display_buffer = bytearray(width * height * 2)  # 2-bytes per pixel (RGB565)
    display = BreakoutColourLCD240x240(display_buffer)
    
    # reads from Pico's temp sensor and converts it into a more manageable number
    sensor_temp = machine.ADC(4)
    conversion_factor = 3.3 / (65535)
    temp_min = 25
    temp_max = 60
    bar_width = 5
    
    # Set the display backlight to 50%
    display.set_backlight(0.5)
    
    temperatures = []
    
    colors = [(0, 0, 255), (0, 255, 0), (255, 255, 0), (255, 0, 0)]
    
    def temperature_to_color(temp):
        temp = min(temp, temp_max)
        temp = max(temp, temp_min)
    
        f_index = float(temp - temp_min) / float(temp_max - temp_min)
        f_index *= len(colors) - 1
        index = int(f_index)
    
        if index == len(colors) - 1:
            return colors[index]
    
        blend_b = f_index - index
        blend_a = 1.0 - blend_b
    
        a = colors[index]
        b = colors[index + 1]
    
        return [int((a[i] * blend_a) + (b[i] * blend_b)) for i in range(3)]
    
    while True:
        # fills the screen with black
        display.set_pen(0, 0, 0)
        display.clear()
    
        # the following two lines do some maths to convert the number from the temp sensor into celsius
        reading = sensor_temp.read_u16() * conversion_factor
        temperature = 27 - (reading - 0.706) / 0.001721
    
        temperatures.append(temperature)
    
        # shifts the temperatures history to the left by one sample
        if len(temperatures) > width // bar_width:
            temperatures.pop(0)
    
        i = 0
        for t in temperatures:
            # chooses a pen colour based on the temperature
            display.set_pen(*temperature_to_color(t))
    
            # draws the reading as a tall, thin rectangle
            display.rectangle(i, height - ((round(t)-20) * 4), bar_width, height)
    
            # the next tall thin rectangle needs to be drawn
            # "bar_width" (default: 5) pixels to the right of the last one
            i += bar_width
    
        # draws a white background for the text
        display.set_pen(255, 255, 255)
        display.rectangle(1, 1, 100, 25)
    
        # writes the reading as text in the white rectangle
        display.set_pen(0, 0, 0)
        display.text("{:.2f}".format(temperature) + "c", 3, 3, 0, 3)
    
        # time to update the display
        display.update()
    
        # Run Full Speed!