Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPI Pico & ST7789 Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 702 subscribers
  • Views 21288 views
  • Users 0 members are here
  • st7789
  • rpi pico
Related

RPI Pico & ST7789 Display

scottiebabe
scottiebabe over 4 years ago

I purchased an off brand ST7789 1.3" Display a few months ago and recently decided it was time to try it out.

 

I did not realize it at the time but there isn't a consistent pinout between display boards. As it turns out the board I purchased did not pin out the chip-select (CS) line.

 

The ST7789 display driver will function without a CS line, however you need to configure the SPI mode (idle state, edge polarity) to communicate with the display. In most cases, I suppose that would be easy enough to change the display driver.

 

Now I wanted to make use of this display with a PI Pico and Micropython. Pimoroni provide a Micropython release with a small number additional libraries on top of MicroPython : https://github.com/pimoroni/pimoroni-pico (unlike CircuitPython which is significantly different from MicroPython).

 

I was trying to get their example code for one of their displays: https://shop.pimoroni.com/products/1-3-spi-colour-lcd-240x240-breakout to function with my off brand display. Unfortunately, I could not find a way to change the SPI operating mode of the display driver unless I wanted to compile their distribution from source (which I didn't want to do), the SPI initialization was all buried in C code.

 

An intsructables author provided a wonderful guide to breaking out the chip-select line: https://www.instructables.com/Adding-CS-Pin-to-13-LCD/  Many thanks. In the process of modify my display I learned a few things the hard way:

  • Rotated R1 90' to bypass the NPN switch
  • Tossed R2 away and used this as the CS pad
  • Be carful with getting the display too hot. The adhesive that held the display in place virtually no longer exists now image
  • Be carful cleaning! Or don't clean at all. I ended up relocating the flux residue with isopropyl from the PCB to inside the display housing and its now a little merky image

image

 

After the display modifications the display came to life!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have never used one of these displays before, but I have to say I am impressed. I was able to get 35 FPS out of a 240x240 display running over SPI.

 

I still don't know what the best way to add graphics to the PICO is. The image I showed in the video was created with ffmpeg outputting a raw video frame:

 

ffmpeg -vcodec png -i img.png -vcodec rawvideo -f rawvideo -pix_fmt rgb565 img.raw

 

Of this random image cropped down to 240x240:

image

Loading the image from flash was very slow.

 

Update: Image Loading Speed

The framebuffer for the ST7789 is stored big-endian so when I was loading the Image I had endian swap in python which was really slow. I can endian swap the raw image file format using dd:

dd conv=swab if=img.raw of=img2.raw

Now loading the image is now significantly faster:

t1 = time.ticks_us()
with open('img2.raw', 'rb') as f:
    for j in range(0,240,24):
        display_buffer[480*j:(480*(j+24))] = f.read(240*48)

display.update() # only update display once now, remove those tabs!
print((time.ticks_us() - t1)/1000)

 

Which now runs in 232 ms 85 ms and appears more as a transition animation versus terribly slow code.

 

Update: Overclocking in MicroPython

One can adjust the system clock frequency in MicroPython by issuing the following command:

machine.freq(190_000_000) # set system clock in Hz

 

When MicroPython alters the system clock frequency, it also reconfigures the peripheral clock source from clk_sys to the external crystal oscillator.

image

 

So, if you want to maintain a high-speed SPI clock frequency, you need to set the clock mux back to clk_sys yourself by:

mem32[0x40008000+0x48] = 0x800

 

With the Pico running at 190 MHz I achieved the following:

     Rainbow Spinner: 53 FPS

     FFT Demo: 16 FPS

     Image Load + Draw: 56 ms (49ms letting the garbage collector run before the load)

 

Of course, there are no guarantees this will always work for every Pico and or display.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 4 years ago

    Hi Scott,

     

    Great results! That is impressive performance. They are nice displays, I tried the same model (identical board to yours)  a while back, but with Arduino. However there the SPI code worked without the chip-select (I probably assigned the chip-select to an unused pin, I'd have to check).

    Looks like you're experiencing situations in Python not unlike what I'm experiencing - I'm currently trying to drive a chip which comes with a library on CircuitPython, but it's not a very good library, and I too don't want to compile from source, it defeats the purpose for me because I don't want to maintain the C code for this particular project, so I've had to re-write, but most code out there for microcontrollers is in C, so just porting code becomes quite an effort if it needs converting to Python.

    I kind-of got it working but there's enough of a discrepancy that I now have to compile in C anyway (I will stub out stuff and compile to run on my PC), so I can compare the two! So, double the work, although the ultimate aim was to make it simpler for the end-user who can then modify the Python code more easily than the C code.

     

    Regarding graphics, when I tried that display, since I was coding in C, I used a C array and it became a permanent part of the executable, not ideal admittedly but then I didn't need a file system etc. I probably used an online tool to convert from (say) .bmp to the C array, but I can't recall for sure now. I guess it could be possible to have a Python list but it might be inefficient (no idea).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to shabaz

    I would absolutely agree I am having a similar experience with uPython. It has been extremely easy to do the things that already work and are well documented and tested. However for any task that is not supported out of the box Its a bit of a mixed bag.

     

    Graphics:

    I'm not sure why the framebuffer is endian-swaped, that could have been done in a PIO SM, however its free code that does work so I can't really complain.

     

    I though maybe I could draw a screen template in inkscape and load that as a base canvas into the framebuffer and then overlay some basic text as needed. However I can't allocate 2 display buffers of 240x240x2 bytes in uPython. The Pico has the memory, so in C I would have been able to do this. But now that I have pre endian swaped the image the load time is quick enough, I think.

     

    Still all things consider this is pretty amazing. These are really are beautiful little displays even with some flux residue in it image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 4 years ago in reply to shabaz

    I would absolutely agree I am having a similar experience with uPython. It has been extremely easy to do the things that already work and are well documented and tested. However for any task that is not supported out of the box Its a bit of a mixed bag.

     

    Graphics:

    I'm not sure why the framebuffer is endian-swaped, that could have been done in a PIO SM, however its free code that does work so I can't really complain.

     

    I though maybe I could draw a screen template in inkscape and load that as a base canvas into the framebuffer and then overlay some basic text as needed. However I can't allocate 2 display buffers of 240x240x2 bytes in uPython. The Pico has the memory, so in C I would have been able to do this. But now that I have pre endian swaped the image the load time is quick enough, I think.

     

    Still all things consider this is pretty amazing. These are really are beautiful little displays even with some flux residue in it image.