Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi imager allows configuration of headless OS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 702 subscribers
  • Views 5090 views
  • Users 0 members are here
  • imager
  • raspberrypi
  • headless
  • sdcard
Related

Raspberry Pi imager allows configuration of headless OS

Jan Cumps
Jan Cumps over 4 years ago

I usually install a headless Raspberry OS on a Pi. I don't use them as desktop/GUI devices.
In the past, getting these activated was a bit involved.

  • ssh disabled
  • wifi not active
  • wrong keyboard for non-US 

To get this set up, I'd usually connect the Pi wired to my network, and put a file called ssh in the root.
Then, I'd check my router for the IP, and use a terminal to set the wifi and keyboard.
Then I'd reboot and start with the other configurations.

Today I Learned that this can now be done via the Raspberry Pi imager.
When you select OS and SD Card, there's an option box.
You can now set the parameters above, and more, up front when creating the image.

Do it before starting to write, because these are set as part of that process.

image

That's all - just wanted to share a new learning.
Since I stumbled on it, I found many tutorials (like this one) that explain it.

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    ntewinkel over 4 years ago

    Thanks for that info, Jan!

    I don't do it very often, but it does get cumbersome to dig out the extra HDMI cable and do the gymnastics around the back of my monitor to hook things up, and then I usually put off dealing with it. Smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 4 years ago

    Thanks for that info, Jan!

    I don't do it very often, but it does get cumbersome to dig out the extra HDMI cable and do the gymnastics around the back of my monitor to hook things up, and then I usually put off dealing with it. Smile