Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum How to solder fairy light strings
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 701 subscribers
  • Views 7997 views
  • Users 0 members are here
Related

How to solder fairy light strings

scottiebabe
scottiebabe over 4 years ago

I have been experimenting with tri-state multiplexing with the Rp2040's PIO statemachine and have found good success.

The PIO code is quite interesting in that its quite different from how I might write it in c-code in a repeating ISR. I may write a blog about it in the future, but here is the code:

# Tri-state multiplexing with done with PIO statemachine
# -scottiebabe 2022
import time
from machine import Pin
import rp2

# Ensure pin pull-ups and pull-downs are disabled
# So pin is Hi-Z when set as input
Pin(0,Pin.IN)
Pin(1,Pin.IN)
Pin(2,Pin.IN)

@rp2.asm_pio(out_shiftdir=rp2.PIO.SHIFT_RIGHT,set_init=[rp2.PIO.OUT_LOW]*3,out_init=[rp2.PIO.OUT_LOW]*3)
def charlie():
    pull(noblock)
    mov(x,osr)
    # Set Pin0 & Pin1 as outputs
    in_(null,2)
    in_(osr,1) # output state of LED0 on Pin0
    out(null,1)
    set(pindirs, 0b011)
    mov(pins, isr) [7]
    in_(null,1)
    in_(osr,1) # output state of LED1 on Pin1
    in_(null,1)
    out(null,1)
    mov(pins, isr) [7]
    
    # Set Pin0 & Pin2 as outputs
    in_(null,2)
    in_(osr,1) # output state of LED2 on Pin0
    out(null,1)
    set(pindirs, 0b101)
    mov(pins, isr) [7]
    in_(osr,1) # output state of LED3 on Pin2
    in_(null,2)
    out(null,1)
    mov(pins, isr) [7]

    # Set Pin1 & Pin2 as outputs
    in_(null,1)
    in_(osr,1) # output state of LED4 on Pin1
    in_(null,1)
    out(null,1)
    set(pins,0)
    set(pindirs, 0b110)
    mov(pins, isr) [7]
    in_(osr,1) # output state of LED5 on Pin2
    in_(null,2)
    out(null,1)
    mov(pins, isr) [7]


# Create the StateMachine with the charlie program, outputting on Pins 0-2.
sm = rp2.StateMachine(0, charlie, freq=20000, set_base=Pin(0),out_base=Pin(0))

# Put bitmap into pio statemachine
sm.put(0b101)

# Start the StateMachine.
sm.active(1)

i = 0
while True:
    i += 1
    sm.put(i % 64)
    time.sleep(0.1)

I would like to try and make my own fairly light strings with three wires and 6 LEDs, similar to these

image

What do you think the best way to solder the LEDs to wires would be?

I'm thinking maybe use a piece of perfboard to hold everything in place while soldering

image

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    0 scottiebabe over 4 years ago

    In the 2-wire fairy lights they appear to use 0603 LEDs as well.

    image

    I really like the wire they use, I don't know where to source that just yet.

    I think a dap of hot glue would be close enough to what is done commercially. I am guessing it may be some type of UV curing epoxy? Or maybe I didn't heat it up enough for the glue to melt... 

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scottiebabe
    0 scottiebabe over 4 years ago

    In the 2-wire fairy lights they appear to use 0603 LEDs as well.

    image

    I really like the wire they use, I don't know where to source that just yet.

    I think a dap of hot glue would be close enough to what is done commercially. I am guessing it may be some type of UV curing epoxy? Or maybe I didn't heat it up enough for the glue to melt... 

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 4 years ago in reply to scottiebabe

    That looks like epoxy, for example Araldite has the consistency that would naturally form a blob shape for such a size of blob. I really like Araldite although for many small blobs a jig would be required to apply it before it all sets (at least for the 5-minute epoxy version). 

    I also like using the stuff in the photo below a lot, although it is not actually glue, it won't stick hard to other materials. The instructions state to put it into boiling water, but it's easier to heat the granules with a hot air tool. Then it is just pressed into shape with fingers (it is not too hot), and there is a good 20-30 seconds time to do that before it cools. If that is not enough time, it can simply be reheated. Each granule is maybe 3mm sphere (I have not measured them).

    image

    Here two granules were used to surround an 0805 sized component, to make solderable 'scope probes. The color is white and only slightly translucent, but perhaps if only one granule was used per component, then it could just surround all sides except the light emitting side.

    image

    It dries rock-hard, so there won't be any proper flexible strain relief as such, except that it would support the wire away from the join, so that's an amount of effective strain relief.

    The Polydoh material is great for making connector backshells, e.g. it can convert a pin header into a pluggable connector : )  

    Anyway, it could be an option, although I think normal epoxy would work great too.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 4 years ago in reply to shabaz

    This polydoh looks like a very handy material to have on hand, and a small quantity should go a long ways for electronics uses. It seems to also be advertised a a tooth repair kit or thermal mold, but it appears to be available for under $20.

    Thanks for the recommendation!  

    I tried hot glue on wax paper,

    image

    It is okay in that it provides a good bond to the wires and LEDs and is mostly transparent, but it doesn't look that pretty...

    • Cancel
    • Vote Up +3 Vote Down