Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help. Very confused about RP2040 PIO.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 24 replies
  • Subscribers 702 subscribers
  • Views 17546 views
  • Users 0 members are here
  • help
  • raspberry_pi
  • rp2040
  • PIO
Related

Help. Very confused about RP2040 PIO.

uncountable
uncountable over 4 years ago

Hi All,

I have a very simple protocol I am trying to implement in the RP2040 PIO module. But I can't make heads or tails of the documentation from the datasheet. There is also not a single helpful example anywhere that I can find. If there is an expert on this board who could give me a couple hints of how I can do the following, I would be very appreciative.

I have a very simple protocol. I have a 6 bit bus. I need to run that bus at half the system clock (66.5 MHz). I have another pin that is the clock, which needs to toggle at system speed. (133 MHz) So an incredibly straightforward and simple, 6 bit, parallel bus streaming continuously at 66.5 MHz.  Now, I have a big block of RAM with data that I need to send out over this bus.  All I am trying to do is understand how to get these FIFO's and shift registers to do what they need to do. Unfortunately, every PIO example seems to assume that your data width is a divisor of 32.  But I don't have that.  Consider, during the first 5 clocks, I will clock out 30 bits. Now I have 2 bits left in my shift register. 

I need to understand how I can transfer, say 16 bits, from the FIFO into my shift register, so that it refills to 18 bits. I can't simply throw away those extra bits I haven't used yet. There is not a single example that I can find in any of the documents that even discusses this issue. I thought maybe I could use 3 state machines each doing 2 bits, but that doesn't work either because I can't get 3 state machines to pull from the same shift register. Maybe there is some complicated way I can tie 3 scripts together at the boundary and keep them perfectly synchronized, but then I need to be very careful to make sure DMA loads the right 32 bit word into the right FIFO at the right time, especially at startup.

What looked like a very simple and elegant solution to my problem now appears to be completely impossible due to the severe limitations of the PIO. Am I missing something about how this works? I am really surprised that the documentation around this peripheral is so dreadful, because the rest of the datasheet and SDK is actually quite good.

I would love to hear any advice or possible solutions from somebody with experience in this area. I can't change the data ordering in RAM. I can barely keep the pipeline full as it is using both cores at 90%. I really hate to abandon the part, because at the price point nothing else can touch it.

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 4 years ago

    Hi,

    I know very little (~0) about the PIO, so I may be talking complete nonsense. As I understand, the FIFOs' are 32-bit wide, and are only ever transferred in 32 bits at a time, i.e. it's impossible to pass in just 16 bits into the shift register. I think you're right, either some scheme to use multiple state machines would be needed, which I can't think of but could be possible, or alternatively you may need to consider a solution where the data ordering in RAM can be changed (I know you stated you cannot, but perhaps it's ok to ignore some parts of the RAM content, so that you're not reordering as such, but loading in data while throwing away some bits: for instance, would it be possible to just use 8 outputs instead, and ignore two of them. In other words, two bits, or 25% of throughput would be effectively wasted, but I guess that may not matter, since all you're concerned about is the 6 bits. But it would require losing two bits of RAM per byte.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 4 years ago

    Hi,

    I know very little (~0) about the PIO, so I may be talking complete nonsense. As I understand, the FIFOs' are 32-bit wide, and are only ever transferred in 32 bits at a time, i.e. it's impossible to pass in just 16 bits into the shift register. I think you're right, either some scheme to use multiple state machines would be needed, which I can't think of but could be possible, or alternatively you may need to consider a solution where the data ordering in RAM can be changed (I know you stated you cannot, but perhaps it's ok to ignore some parts of the RAM content, so that you're not reordering as such, but loading in data while throwing away some bits: for instance, would it be possible to just use 8 outputs instead, and ignore two of them. In other words, two bits, or 25% of throughput would be effectively wasted, but I guess that may not matter, since all you're concerned about is the 6 bits. But it would require losing two bits of RAM per byte.