Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What Raspberry Pi Pico development board do you recommend
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 700 subscribers
  • Views 16450 views
  • Users 0 members are here
  • raspberry pico
  • pico
  • development_kit
Related

What Raspberry Pi Pico development board do you recommend

colporteur
colporteur over 3 years ago

Can you share some of your Pico insight? I'm looking to start dabbling in Pico. I have experience with Pi's and Arduino's and look forward to discovering the Pico.

My experience suggests a development board is an ideal platform to begin with. It removes some of the heavy liftings. Yeah I could breadboard it and work from there but I thought, hey Christmas is coming why not get yourself a new toy. Who wouldn't want a slick development board under the tree?

Does anyone have any suggestions? What is good or bad in a development board? Since I don't know what I am looking for maybe a list from others is a good starting point?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi Sean,

    I'm biased too, but if you want the DIY option, then in https://github.com/shabaz123/pico-eurocard there is a zip file there called exportpico_euro_v_2_0.zip.

    If that file is sent to a PCB factory, then the board that arrives can be used as-is (apart from buying the Pico), since the Pico is very complete.

    In other words, by just soldering on the Pi Pico (either directly or with header pins), then the board can be used to patch wires to external breadboard, or to the perfboard area already on the PCB.

    Then, whenever you feel like it, additional parts can be soldered on depending on needs. For instance, a couple of buttons and LEDs, or a 3.3V or 5V regulator, if you want to power other things too.

    This is the completely populated board (but as mentioned, you could start with just the Pico soldered on). The board has space for two Picos (thanks to an idea from Jan Cumps  ). The second Pico is a smaller XIAO RP2040 (it is just used as a debugger when C/C++ coding using the Pico SDK. If you're using Arduino or Python, then it's not required.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 3 years ago in reply to shabaz

    Is your board something Newark / element14 will be (is already?) stocking? Is that a possibility, cstanton  ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to ntewinkel

    I wish/hope they can but I don't know who to ask. Since not everyone will want 5-10 boards from a PCB manufacturer and the associated shipping costs from China, it would be useful for people to buy just one or two.

    I quite like the large size, since it has the built-in debugger and power supplies. Kind of all-in-one for projects. 

    The one that Gough Lui links is interesting too, I just noticed they have LEDs on all ports which is pretty neat. I was just thinking, there is a cheaper way to do that using a different method on the Pico-Euro board. On the right side of the Pico-Euro board, the outputs are ordered on consecutive pins, since this is useful for PIO projects (PIO benefits from ordered pins). It is easy to connect a logic analyzer on banks of pins, but there could also be a plug-on custom PCB with LEDs on it (e.g. 8 LEDs), that can be removed and connected to different banks of 8 pins when desired. Far lower cost to do that than having dozens of MOSFETs and LEDs soldered.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to ntewinkel

    I wish/hope they can but I don't know who to ask. Since not everyone will want 5-10 boards from a PCB manufacturer and the associated shipping costs from China, it would be useful for people to buy just one or two.

    I quite like the large size, since it has the built-in debugger and power supplies. Kind of all-in-one for projects. 

    The one that Gough Lui links is interesting too, I just noticed they have LEDs on all ports which is pretty neat. I was just thinking, there is a cheaper way to do that using a different method on the Pico-Euro board. On the right side of the Pico-Euro board, the outputs are ordered on consecutive pins, since this is useful for PIO projects (PIO benefits from ordered pins). It is easy to connect a logic analyzer on banks of pins, but there could also be a plug-on custom PCB with LEDs on it (e.g. 8 LEDs), that can be removed and connected to different banks of 8 pins when desired. Far lower cost to do that than having dozens of MOSFETs and LEDs soldered.

    • Cancel
    • Vote Up +4 Vote Down