Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pico Eurocard Rev 2.0 - Free (just pay shipping)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 62 replies
  • Subscribers 702 subscribers
  • Views 12441 views
  • Users 0 members are here
  • pico-euro
  • eurocard
  • pico-eurocard
  • pi pico
Related

Pico Eurocard Rev 2.0 - Free (just pay shipping)

shabaz
shabaz over 3 years ago

EDIT: all gone, but it is easy to build your own, using the more recent (currently rev 2.2) files on GitHub.

(Hoping it is OK to post this, since it's a not-for-profit thing!).

Hi,

I have three Pico Eurocard Rev 2.0 (it's a recent version, with no known issues so far!) build-as-you-go-and-bring-your-own-Pico package : )

A fully populated Rev 2 looks like this:

image

However the build-as-you-go-and-bring-your-own-Pico version requires you to bring your own Picos', and it can be immediately used, but it is missing stuff that can be added later, such as the voltage regulator modules and microSD card socket. 

The board has all surface-mount Rs, Cs and the single MOSFET pre-soldered, since they would be a pain to ship unassembled, due to the small size.

The package includes a bag of through-hole parts, but it doesn't include header pins/sockets and DC-DC converter, DC jack and microSD socket. Those are all easy to locally source, and are not essential, to use; just a Pi Pico is required, but you may wish to also get some header pins as well. Then, if you need (say) more 3.3V capability, then you could buy a 3.3V regulator (it's just a couple of £) and add it on.

These are spare boards, I don't want to charge anything for them. If you feel uncomfortable with that, then I'll accept the cost of the raw PCB and components, which let's say is £5. But I will only accept that so people don't feel uncomfortable accepting a free item : ) but there's no obligation to pay - just pay for the shipping. I will have to declare the nominal £5+shipping on the customs form however.

There's no warranty, and no returns since this wouldn't be a very good business venture to sell at no profit : ) and it's an experimental board and I'm not charging or warranting the SMD assembly either : ) However as mentioned, it's unlikely there will be any fault (and I took ESD precautions soldering the SMD parts).

The photo here shows everything that is included.

image

This is the contents of the bag of through-hole bits:

image


Tracked shipping (from UK) will be £15 USA, £10 in Europe, and let's say £5 UK, and I will use parcel2go.com.

Example, USA shipping:

image


Please use the parcel2go.com website to see the quote for any other country (courier collection, tracked please!).

If you're interested, please leave a comment telling me, and then send me a private message with the shipping address (or click to connect and then send me the shipping address). There are only three boards as mentioned (one per person), and I'm unlikely to build more by hand : ) 

In terms of payment, I have no convenient mechanism for this that I wish to use, but instead we could barter for say coffee vouchers : ) for instance costa e-gift using https://gifting.costa.co.uk/
I'll send you my e-mail address for that.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    I figured I may as well solder the through-hole parts too, it beats sending a bag of bits (sorry if anyone was looking forward to the assembly!) - although, there's still a bit of assembly to do, since I didn't have all the parts, but all the boards are usable (just add Pico).

    Two of the boards have the micro SD card socket (I only had two sockets) and sockets ready for the Pico, but one board doesn't, it will need SIL sockets soldered on (or directly solder the Pico to it, but it's better to use a socket so that the board can be used for the normal Pico, as well as Pico Wireless, both will work. However for that board, I've soldered in a 5V regulator module, and have a rotary encoder for that board too, so they are all approx equal, give or take a few bits.

    All of the boards are ready to use, but if you require more 5V or 3.3V power, then it's good to add the DC-DC converter modules to the board (as mentioned one board already has the 5V DC-DC converter installed, it's visible on the left side of the lower board. 

    For anyone wishing to use the Pico C SDK, then soldering on a XIAO RP2040 (there is space for it on the top-right right side of the board) is definitely worthwhile, it speeds the development effort a lot. For Arduino or Python coding, the XIAO board is not used.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to shabaz

    Wow, awesome support for the community.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to dougw

    Hi Doug,

    Thanks!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to dougw

    Hi Doug,

    Thanks!