Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pico Eurocard Rev 2.0 - Free (just pay shipping)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 62 replies
  • Subscribers 700 subscribers
  • Views 12464 views
  • Users 0 members are here
  • pico-euro
  • eurocard
  • pico-eurocard
  • pi pico
Related

Pico Eurocard Rev 2.0 - Free (just pay shipping)

shabaz
shabaz over 3 years ago

EDIT: all gone, but it is easy to build your own, using the more recent (currently rev 2.2) files on GitHub.

(Hoping it is OK to post this, since it's a not-for-profit thing!).

Hi,

I have three Pico Eurocard Rev 2.0 (it's a recent version, with no known issues so far!) build-as-you-go-and-bring-your-own-Pico package : )

A fully populated Rev 2 looks like this:

image

However the build-as-you-go-and-bring-your-own-Pico version requires you to bring your own Picos', and it can be immediately used, but it is missing stuff that can be added later, such as the voltage regulator modules and microSD card socket. 

The board has all surface-mount Rs, Cs and the single MOSFET pre-soldered, since they would be a pain to ship unassembled, due to the small size.

The package includes a bag of through-hole parts, but it doesn't include header pins/sockets and DC-DC converter, DC jack and microSD socket. Those are all easy to locally source, and are not essential, to use; just a Pi Pico is required, but you may wish to also get some header pins as well. Then, if you need (say) more 3.3V capability, then you could buy a 3.3V regulator (it's just a couple of £) and add it on.

These are spare boards, I don't want to charge anything for them. If you feel uncomfortable with that, then I'll accept the cost of the raw PCB and components, which let's say is £5. But I will only accept that so people don't feel uncomfortable accepting a free item : ) but there's no obligation to pay - just pay for the shipping. I will have to declare the nominal £5+shipping on the customs form however.

There's no warranty, and no returns since this wouldn't be a very good business venture to sell at no profit : ) and it's an experimental board and I'm not charging or warranting the SMD assembly either : ) However as mentioned, it's unlikely there will be any fault (and I took ESD precautions soldering the SMD parts).

The photo here shows everything that is included.

image

This is the contents of the bag of through-hole bits:

image


Tracked shipping (from UK) will be £15 USA, £10 in Europe, and let's say £5 UK, and I will use parcel2go.com.

Example, USA shipping:

image


Please use the parcel2go.com website to see the quote for any other country (courier collection, tracked please!).

If you're interested, please leave a comment telling me, and then send me a private message with the shipping address (or click to connect and then send me the shipping address). There are only three boards as mentioned (one per person), and I'm unlikely to build more by hand : ) 

In terms of payment, I have no convenient mechanism for this that I wish to use, but instead we could barter for say coffee vouchers : ) for instance costa e-gift using https://gifting.costa.co.uk/
I'll send you my e-mail address for that.

  • Sign in to reply
  • Cancel
Parents
  • baldengineer
    baldengineer over 3 years ago

    Update, I received my Pico-Eurocard! Thank you again Shabaz!!

    I am still waiting for a replacement Xiao (I thought I ordered a new one... I did not!)

    But in the meantime, I loaded CircuitPython and made some blinky happen.

    pi pico in a carrier board blinking yellow and amber LEDs

    I plan to do some exploration with FreeRTOS very soon. I'm looking forward to using the Dev Board while I do that.

    Thanks again! You did a great job on the board. And I really appreciate the effort of including printed instructions!

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to baldengineer
    baldengineer said:
    I am still waiting for a replacement Xiao (I thought I ordered a new one... I did not!)

    If you manage to get one, it 'll be an asset. You can program it with shabaz ' version of the PicoProbe firmware.
    This will give you the luxury of having a programmer/debugger like many commercial boards,
    and you can power simple designs from the Xiao - including the Pico mounted on the eurocard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    It was Jan's idea to add a debugger, and it is frankly brilliant, it has improved coding/testing speed a lot, no boot buttons to press, and it's all quick. There's a jumper at the top-right of the board for the occasions where you are in-the-zone just programming, and want to power everything off the single USB-C cable connected to the Xiao. The PicoProbe firmware is here (file called picoprobe_xiao.uf2)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to Jan Cumps

    I'm looking forward to experimenting with picoprobe firmware and the Xiao.

    I have a J-Link Mini, which is what I've used with my other RP2040 projects. But, those also have the small-pitched connector the J-Link Mini uses to go with them.

    So, connecting to a Pico isn't convenient (even with an adapter board.)

    Also, I'm always worried about damaging the J-Link, since they're nearly impossible to get right now.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 3 years ago in reply to Jan Cumps

    I'm looking forward to experimenting with picoprobe firmware and the Xiao.

    I have a J-Link Mini, which is what I've used with my other RP2040 projects. But, those also have the small-pitched connector the J-Link Mini uses to go with them.

    So, connecting to a Pico isn't convenient (even with an adapter board.)

    Also, I'm always worried about damaging the J-Link, since they're nearly impossible to get right now.