Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Pico Eurocard - SD Card signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 701 subscribers
  • Views 4577 views
  • Users 0 members are here
  • pico
  • pico_eurocard
  • fatfs
Related

Pi Pico Eurocard - SD Card signals

Jan Cumps
Jan Cumps over 3 years ago

follow up of an earlier discussion: what do the SD Card signals look like on an oscilloscope.

image

I've made these connections with the oscilloscope:

EuroCard Pico pin function channel
*CS IO13 SPI1 CSn 4 dark blue
MOSI IO11 SPI1 TX 2 light blue
SCLK IO10 SPI1 SCK 1 yellow
MISO IO12 SPI1 RX 3 magenta

All channels are set to 2 V/div. Here are the results of the start of a communication.:

image

image

image

All 3 scope captures are based on a single sample. Just different locations and time-base views.
This is the old sloppy sample that Michael refers to in the 1st comment:

image

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    One of the dev board advantages, is that you can measure current of the Pico fairly easy. By using external power (can be the PicoProbe or one of the options at the left side of the board). And using a current meter instead of a jumper.

    image

    This is the envelope when activating the SD card and do some reads/writes.
    For real low power designs* you may want to remove the LED, and pull-ups of peripherals you don't use.

    * pico MCU in its current version isn't targeting very low power. An upside of that is that it's a bit easier to start learning to collect power consumption data with it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    Just thinking, if the ADC in the RP2040 is any good (I've not used it), then there's an argument for making the Picoprobe do a bit more, and take current readings too : ) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    It's not that good. In the current silicon design, the ADC is the known sick baby. There's an errata for it, but not a solution.

    Good enough for some current sampling though.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    It's not that good. In the current silicon design, the ADC is the known sick baby. There's an errata for it, but not a solution.

    Good enough for some current sampling though.

    • Cancel
    • Vote Up +4 Vote Down