Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Pico Eurocard - SD Card signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 703 subscribers
  • Views 4536 views
  • Users 0 members are here
  • pico
  • pico_eurocard
  • fatfs
Related

Pi Pico Eurocard - SD Card signals

Jan Cumps
Jan Cumps over 3 years ago

follow up of an earlier discussion: what do the SD Card signals look like on an oscilloscope.

image

I've made these connections with the oscilloscope:

EuroCard Pico pin function channel
*CS IO13 SPI1 CSn 4 dark blue
MOSI IO11 SPI1 TX 2 light blue
SCLK IO10 SPI1 SCK 1 yellow
MISO IO12 SPI1 RX 3 magenta

All channels are set to 2 V/div. Here are the results of the start of a communication.:

image

image

image

All 3 scope captures are based on a single sample. Just different locations and time-base views.
This is the old sloppy sample that Michael refers to in the 1st comment:

image

  • Sign in to reply
  • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    These waveforms look a bit odd - is that noise on the MOSI line ?

    Is the 11 clock pulses folowed by clock staying high an SD card thing - ?

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett

    that was all my extreme sloppy sampling. I just turned on the scope, put all to 2V, and settled for the first image I could replicate. Channel 2 and 3 were on AC

    I've made new samples - 3 this time. With deep memory on so that I had meaningful info.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to Jan Cumps

    Looks much better now - I can believe that might work !

    You get the opposite problem when you use a logic analyser, since the input is just a comparator all the pulses look perfect, and sometimes they really are like your first scope plot.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    Very neat! Great work. I want to experiment with some of these fancy new Pseudostatic RAM memory chips that have a QSPI flash interface.

    image

    If I mod wire this in place of the on pcb flash  on a Pico, I should have 8 MB of RAM! Of course I would have to load the code over the swd interface....

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to scottiebabe

    Nice chip. did you mean to pick the 1.8V one ?

    (They do 3.3V as well.)

    I have a socket on a board which can take the Microchip 1Mbit serial RAM but this one is a good bit nicer, and cheap and in stock !

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to michaelkellett

    I don't know why the 3V version didn't show up in my search but as you say it is there too!

    image

    The ESP32-cam stores its image framebuffer on a PSRAM chip. The teensy 4.1 lets you choose your chip if you so desire:

    image

    https://www.pjrc.com/store/psram.html 

    Its a technology too good to ignore, I need to learn more of the nitty gritty details...

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Hi Jan,

    That's great to see what the signals look like. Neat work with the probes in the cramped space : ) 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    Yes, the MISO looks healthy to me, without a pull-up:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    For perspective, the first frame, and the start of the second frame, when starting the "simple" test of the test program I'm running. The ~CS being low on CH4 indicates the boundaries of a frame.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    A full cycle: check if a file exist. read, recreate, write lines, close

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>