Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Probing the RP2040 QSPI Flash Interface
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 703 subscribers
  • Views 14198 views
  • Users 0 members are here
Related

Probing the RP2040 QSPI Flash Interface

scottiebabe
scottiebabe over 3 years ago

As you know SD Cards are bigger Divas than me! With latencies of up to several hundreds of milliseconds and the complexity of a file they can be trying to deal with at times. Not to mention, I don’t usually need gigabytes of storage.

Today there are so many memory chips with a simple SPI interface available. You can get several megabytes of flash/f-ram/psram in an 8-pin package for a dollar or two.

So, I am just trying to learn more about these QSPI memory chips.

I guess the best place to start is by probing known working designs, like the many RP2040 development boards like the RPI Pico or Adafruit’s RP2040 feather.

When the RP2040 comes out of reset it begins execution of its internal bootrom code:

https://github.com/raspberrypi/pico-bootrom/blob/master/bootrom/bootrom_main.c

Where it tries to initialize an SPI memory IC over its SSI interface. It does this by trying to read the first 256 bytes with different CPOL CPHA combinations and looking for a valid second stage bootloader image.

image
image

The last 4 bytes of the 256 byte page are a checksum that the Rp2040 uses to validate that a second stage boot image was found.

image

The RP2040 starts executing the loaded second stage bootloader image and eventually gets ready to start running of external flash.

image

Just before switching over from the 1-bit xx25 interface to QuadSPI the firmware reads status register 2:

image

To switch over to using “Quad I/O Fast Read with Continuous Read Mode” The 0xEB command is sent:

image

With command bits M5-4 = (1,0) subsequent flash reads can omit the command portion:

image

The unfortunate part for me is, I don’t have a QSPI protocol decoder (though it appears neither does a $20,000 oscilloscope *shakes head*). Using a clocked parallel bus decoder gets me close enough I suppose:

image
image

It isn’t too difficult to follow along:

image

For some reason micropython compiled for an Adafruit feather never switches over to QSPI, So in that case I get a nice tabular report using a SPI memory protocol decoder:

image

It is looking quite likely I might be able to boot an RP2040 off an 8MB PSRAM chip in 1-bit SPI mode.

I don’t know enough yet to know how common the QuadIO mode commands and wait cycle counts are between chips.

Thanks for reading Slight smile

Onwards and upwards!

  • Sign in to reply
  • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to michaelkellett

    Ooh that is extra fancy!!!

    I'm not sure I am against having my scope sample the signal, but I agree with you I much preferer  examining/analyzing digital data on my PC!

    I tried downloading the zeroplus software to see if I could import a csv file, but no luck! O well can't blame them for making one purchase the product to use their software. 

    I also noticed they have a glitch filter included. Neither digilent or opensource pulse view do that for you. My protocol decoders were quite upset see the chipselct line toggle mid transaction... But it happens with fast edges and big long hookup leads. I added a zerophase lowpass filter in matlab to deglitch the signals from crosstalk.

    I love the reset button in the machinist vice! Classy! 

    I am amazed you were even able to buy an FPGA at all, looks like a really neat project Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Excellent prototyping techniques! I am excited to follow along Slight smile Great work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to michaelkellett

    I use a lot of vises, but I obviously don't have enough of that type - they look very handy.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to scottiebabe

    It is good idea. I recommend trying this platform. Note that Kit provided as part of challenge has no FRAM but it has FLASH, so you can apply probes and see how it works.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to scottiebabe

    If you are looking for small cheap and avaialble FPGAs right now then your best bet is Efinix.

    You need to fork out £65 for a dev board to get a software license but once you have done that Digikey have tens of K parts in stock:

    eg Trion 8 (8k LUT in TQFP144), 54057 parts in stock or Trion 20 (20k LUT in TQFP144), 20700 parts in stock at £13.20 each (1 off price)

    I'm working on a test board with a T20 and two of the PSRAM chips and a few other bits. (Because I need to have one on a board of my own and working before I can really recomend to paying customers that they design it in to a product.)

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to dougw

    I bought these (two small and one large) half price quite recently from my usual metalwork tool supplier. I wasn't sure if they would be useful but they are so nice to use that I think I might even buy some more !

    I'll wait until they next have them on offer.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    They are a little too pricey for me:

    image

    But, they look wonderful!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    The reason my feather rp2040 boots in potato mode:

    This enables you to boot from almost anything: you can pretty much solder a potato to your PCB, or a piece of cheese

    The tradeoff is performance around 3x worse than QSPI XIP

    Source: https://github.com/raspberrypi/pico-sdk/blob/master/src/rp2_common/boot_stage2/boot2_generic_03h.S 

    Is adafruit never submitted a flash configuration back into the pico-sdk. So projects using the pico-sdk boot in the legacy 1-bit serial SPI memory format. It is my understanding that almost all xx25 have the same read/write commands in 1bit spi mode.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    There are very low-cost aluminium versions, not precise : ) but good for holding boards or components. They are really handy, I like using this style of vise too. Quite a lot more lightweight, so it isn't as good for building up a slightly more rugged test scenario as the proper tool vises however.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>