Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Probing the RP2040 QSPI Flash Interface
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 703 subscribers
  • Views 14191 views
  • Users 0 members are here
Related

Probing the RP2040 QSPI Flash Interface

scottiebabe
scottiebabe over 3 years ago

As you know SD Cards are bigger Divas than me! With latencies of up to several hundreds of milliseconds and the complexity of a file they can be trying to deal with at times. Not to mention, I don’t usually need gigabytes of storage.

Today there are so many memory chips with a simple SPI interface available. You can get several megabytes of flash/f-ram/psram in an 8-pin package for a dollar or two.

So, I am just trying to learn more about these QSPI memory chips.

I guess the best place to start is by probing known working designs, like the many RP2040 development boards like the RPI Pico or Adafruit’s RP2040 feather.

When the RP2040 comes out of reset it begins execution of its internal bootrom code:

https://github.com/raspberrypi/pico-bootrom/blob/master/bootrom/bootrom_main.c

Where it tries to initialize an SPI memory IC over its SSI interface. It does this by trying to read the first 256 bytes with different CPOL CPHA combinations and looking for a valid second stage bootloader image.

image
image

The last 4 bytes of the 256 byte page are a checksum that the Rp2040 uses to validate that a second stage boot image was found.

image

The RP2040 starts executing the loaded second stage bootloader image and eventually gets ready to start running of external flash.

image

Just before switching over from the 1-bit xx25 interface to QuadSPI the firmware reads status register 2:

image

To switch over to using “Quad I/O Fast Read with Continuous Read Mode” The 0xEB command is sent:

image

With command bits M5-4 = (1,0) subsequent flash reads can omit the command portion:

image

The unfortunate part for me is, I don’t have a QSPI protocol decoder (though it appears neither does a $20,000 oscilloscope *shakes head*). Using a clocked parallel bus decoder gets me close enough I suppose:

image
image

It isn’t too difficult to follow along:

image

For some reason micropython compiled for an Adafruit feather never switches over to QSPI, So in that case I get a nice tabular report using a SPI memory protocol decoder:

image

It is looking quite likely I might be able to boot an RP2040 off an 8MB PSRAM chip in 1-bit SPI mode.

I don’t know enough yet to know how common the QuadIO mode commands and wait cycle counts are between chips.

Thanks for reading Slight smile

Onwards and upwards!

  • Sign in to reply
  • Cancel
  • dougw
    dougw over 3 years ago in reply to scottiebabe

    Me too. I just ordered a plastic one and cheap aluminum one to tide me over until a decent sale comes along.

    image

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Interesting! Seems they like taking shortcuts. Incidentally, and unrelated, CircuitPython seems to have a vulnerability window, where if you power-off the Pico during start-up, there's a high risk that there will be corruption. After experiencing that (I reported it and they managed to reduce the window, but still..) and several other issues and bugs throughout, I decided to avoid CircuitPython. It's a shame because it is feature-rich, but at the expense that not everything is reliable.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    Those rubber bumpers look really handy too! I found one that comes with a set of drill bits too

    image

    Thanks for the tip!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to shabaz

    With a quick release! I suppose you can't have too many of these things! Thanks for the recommendation Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<